Industrial Enclosures for any Application

October 4, 2018 at 8:00 AM

 

When it comes to protecting your valuable equipment, a NEMA enclosure can be a great solution. Whether your equipment could be exposed to the elements, chemicals, human tampering or theft, using an enclosure can ensure your investment is protected and provide you with peace of mind. Different enclosures provide different benefits, and you must find the best fit for your application. Here, we’ll take a closer look at Industrial enclosures and all that they have to offer.

 

When it comes to location, industrial enclosures can be used for both indoor and outdoor applications. In any setting, industrial enclosures provide extra security against theft, tampering and damage. Standard enclosures are lockable and keyed locks can be added as an extra measure to keep valuable components safe. Weatherproof outdoor enclosures can provide superior protection from the elements for outdoor wireless access points and sensitive electric components. Plus, with the option of adding heating and cooling or power, these enclosures deliver dependable performance in any climate.

 

There are numerous features that make industrial enclosures ideal for protecting sensitive equipment, these include mounting plates that securely mount equipment inside an enclosure and a thermostat controlled cooling fan that keeps equipment cool in high temperature environments. Also, a mounting lid can prevent damage and theft of the equipment inside the enclosure, these lids can have hinges, removable lids or clear viewing windows for easier viewing while maintaining security. Power over Ethernet (PoE) interface is another great feature that delivers power to the enclosed equipment where power sources are limited, plus it provides additional surge protection for internal PoE compatible equipment.

 

Many applications can benefit from the use of an industrial enclosure, and while the details might vary, they all share a similar set of requirements that include being able to operate under exceedingly harsh conditions that include exposure to corrosive chemicals, extreme temperatures and more. Some of these applications include industrial automation, oil and gas, and transportation. Rugged, industrial enclosures are also ideal for security and automation applications such as access controls, fire alarms, video surveillance equipment and building automation.  Indoor and outdoor enclosures can be used in a variety of locations to protect equipment, including cell towers and rooftops, open-access basements, telecom closets, shopping centers and factories.

 

Overall, industrial enclosures are a great way to keep expensive equipment safe. In almost any application, and even in the harshest conditions, they provide a level of security that is unmatched. To take a look at L-com’s complete, comprehensive line of industrial enclosures, click here.

 

Case Study: Union Electrica

September 27, 2018 at 8:00 AM

 

Union Electrica, a systems design and installation services company based in Uruguay and servicing all of Latin America, won a large contract with the city of Medellin, Columbia. They were tasked with the challenge of deploying a WiMAX network that connected more than 1,200 subscriber points, but they needed help. Fortunately, L-com had the perfect solution.

 

To successfully complete the WiMAX network rollout in Medellin, Union Electronica needed a system that would support the 3.5 GHz frequency with a focused directional wireless connection that could perform in all weather conditions. They also required low-loss cables and lightning and surge protectors to complete the installation.

 

L-com was able to fulfill all of Union Electrica’s network requirements with a 3.5 GHz antenna that was compact, minimized interference, supported vertical or horizontal polarization and featured a 25° beamwidth.

 

The L-com team also provided low-loss coaxial cable assemblies, surge protectors and COTS antennas and accessories, all of which were in-stock and available for immediate shipment to fulfill the accelerated installation schedule.

 

In the end, with the help of L-com, Union Electrica was able to successfully deliver a high-speed WiMAX network to the city of Medellin while meeting all budget and installation deadline requirements.

 

To read the entire case study click here.

 

Cabling in Medical Devices

September 13, 2018 at 8:00 AM

 

When we think of cabling, we usually think of data and communications and networking, but there are all types of industries and applications that use cabling. The medical field is one of those industries that is increasingly using technology in medical devices, and wiring and cabling have been a large component in the growth of those technological advancements.

 

There are many medical devices that are dependent on interconnect components such as cabling, but unlike cabling used for a communications network, the requirements for medical device cables are somewhat unique. Medical devices cables must be extremely flexible and withstand repeated flexing. They also have to meet stringent regulated safety guidelines that vary depending on what type of device the cable will be used in and how/if it will come in contact with the patient. In addition to constant flexing and safety requirements, these cables also must be able to withstand constant sterilization processes, which include autoclave, gamma and exposure to chemicals and solvents.  

 

Another challenge of medical device cabling is keeping up with devices as they get smaller. For example, MRI machines now fit into a single room, ultrasound machines are now portable on mobile carts and consumer medical devices are handheld. The miniaturization of medical devices has many benefits including increased mobility and diagnostic capabilities, lower power requirements and less distance from the patient. Plus, the miniaturization of cables in these devices results in less cabling weight which makes maneuvering the cables around the patient easier. It also allows for greater flexibility since cabling with a smaller diameter can be tightly bent and still retain the recommended minimum bend radius.

 

Some of the most important cable factors to consider when it comes to cabling in medical devices are reliability, cable jacket, mating design and connector type. When it comes to people’s health, the reliability of a cable can be the difference between life and death. If cables are working properly or the connections aren’t reliable, devices can malfunction and that can cause great harm. With that in mind, cable connectors have to be properly mated, which can be made easier with the use of color-coding or keyed connectors. Plus, cables with alternative contact designs, such as hyperboloid, are good solutions to avoid issues with contact design, and plug-and-play connectors simplify the task of connecting different pieces of equipment. Lastly, selecting the proper cable jacket, whether it needs to be flexible, insulated or able to withstand a corrosive environment is critical to the overall operation of any cable.

 

The medical industry can be a demanding environment for cabling, and there are many requirements to consider, but as this is an industry with technology that is constantly advancing, and so will the need for cables. 

 

The Mighty MPO Connector

August 30, 2018 at 8:00 AM

 

Imagine a connector that can save you time, save you space and still perform – there you have the mighty MPO connector. Multi-fiber push on (MPO) connectors have gained popularity and are the primary multiple fiber connector used globally for high-speed data and telecom communications networks. These mighty connectors come in an array of options and make life easier while delivering the fast speeds needed for today’s technology. Here, we’ll take a look at what makes the MPO connector so mighty.

 

First, let’s look at the design. MPO connectors are designed to combine many fibers in one connector, which reduces the amount of time needed for splicing and connecting fibers, and also saves space. Each connectors has a key on one side. A “key up” position has the key on top, “key down” position has the key on the bottom. Each fiber in the connector is numbered left to right (P1, P2, etc.) and there is a white dot on the connector body to show where position 1 is located.

 

Originally, MPO connectors were only offered as single-row, 12-fiber connectors, but now there are multiple variations available. Today, there are 8 and 16 single-row options that can then be stacked to create 24, 36 and 72 fiber connectors with multiple precision ferrules. Mating these connectors is made simple through the IEC 61754-7 and EIA/TIA-604-5 (FOCSI 5) standards that ensure all MPO connectors meet performance and mateability requirements. Though, keep in mind that the wider connectors and stacked ferrules are susceptible to greater insertion loss and reflection problems because holding the outer fibers alignment tolerances is challenging.

  
 

Now, let’s look at how these mighty connectors perform. As mentioned above, MPO connectors are a popular choice for high-speed telecom and data communications. They have been utilized in duplex 10 Gig fiber applications as a means to ease cable management, save money, speed-up installation and take-up less space. Twelve-fiber MPO connectors can supply six-10 Gig transmit fibers and six-10 Gig receive fibers. Eight-fiber MPOs are capable of 40 Gig speeds and 24 fibers deliver 100 Gig speeds. With connectors able to be combined and stacked to increase speed and capabilities, MPO connectors can deliver the performance specs to keep up with future increased data requirements.

 

As a diverse connector option with great flexibility and ease of use, MPO connectors are a mighty powerful and mighty fine option for many connecting needs and are sure to remain a viable option in the fiber optic marketplace for a long time to come.

 

Next Generation PoE - What You Need to Know

August 23, 2018 at 8:00 AM

 
What’s better than Power over Ethernet? More Power over Ethernet (PoE), of course – and that is exactly what PoE++ is delivering. PoE++ expands upon the traditional PoE benefits of delivering data and power over a single Ethernet cable, it increases power capabilities and extends PoE’s reach into new industries and applications. Here, we’ll tell you exactly what gives PoE++ those two extras plus signs.
 
First, let’s look at a numbers comparison. The first ratified PoE standard 802.3af supports 15.44 watts of power, but power dissipation usually lowers that number to a reliable 12.95 watts. Then PoE+ was introduced and bolstered power to 30.8 watts with the 802.3at standard, though power dissipation usually takes its toll and lowers power to 25.5 watts. PoE++ (the 802.3bt standard) will be capable of supplying more than 3 times the power of PoE+ with up to 100 watts (Type 4) of DC power and the ability to support 10 Gbps connections.
 
Traditionally, PoE has been used in networking applications. With PoE++, the technology’s reach is extended to include healthcare, point of sale, financial and surveillance industry applications. PoE++ utilizes all four twisted pairs of an Ethernet cable for optimal power transmission. It consists of Mode A and Mode B, and combines them to reach higher voltage levels. Mode A is also referred to as Type A, Type 3 or 4-pair PoE. It is specified for 60W, 50W reliable, and is able to support technology such as access controls, point of sale readers, IP cameras and nurse call devices. Mode B is also known as Type B, Type 4 or higher-power PoE. It is designed for 100 watts of power, 80 watts after power dissipation, and increases the capabilities to also include support of videoconferencing systems, laptops, desktops and televisions.
 
PoE++ is slated to bring more power, more conveniently to more devices than ever before. With all of the speed, convenience and capabilities that this new technology offers, it’s no wonder that PoE++ earned those extra plus marks.

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845