How To Amplify Wireless Signals without an FCC Operators License

May 1, 2013 at 10:00 AM

 

Example of a Wireless Amplifier Setup for a Laptop

Do you need a wireless amplifier but can't get one?

 

That's because the Federal Communications Commission (FCC) Part 15 regulations dictate the use of RF power amplifiers in the United States. Individual RF power amplifiers are not offered for general sale within the United States and must be part of a wireless system previously certified by the FCC.

 

Customers in the US that are inquiring about purchasing individual amplifiers must first be prequalified to see if they meet certain requirements. Those who qualify are typically Federal Government agencies, Department of Defense (DOD) and FCC licensed operators. This is obviously not ideal for the typical home or commercial business user.

 

So how can you get one?

 

L-com carries FCC-certified amplifier kits. These kits are complete 2.4 GHz wireless systems that feature a wireless USB adapter, rubber duck antenna and amplifier. Since FCC ID numbers have been granted to these kits, prequalification is not required in order for them to be sold.

 

L-com carries three types of FCC-certified WiFi boosters: standard, economy grade, and PoE compliant. Available with amplifiers ranging from 100 mW to 1 Watt, they provide exactly the boost your signal needs.

 

Click here for a helpful video on how to setup a laptop WiFi booster kit:

 

Wireless Amplifier Video

 

Identifying Array Antennas

April 17, 2013 at 10:00 AM

What are they?


An antenna array is a group of two or more directional (usually panel style) antennas that are grouped together to form an Omni directional signal. Many times an RF splitter is used to connect the multiple antennas to a single access point or WiFi amplifier.

 

The benefit of using an antenna array over a single Omni directional antenna is that the antenna array provides radiation patterns that a single Omni antenna would not. Many times antenna arrays provide greater coverage than a single Omni antenna could.

 

 

Antenna array mounted on a pole RF splitter connected to an antenna array
Antenna array mounted on a pole RF splitter connected to an antenna array

Down tilt mounting feature
Down tilt mounting feature 

 



Where Would You Use Them?


Antenna arrays are used in outdoor point-to-multipoint applications. L-com's antenna arrays are available in 90° (4 panels), 120° ( 3 panels), and 180° (2 panels) configurations and include appropriate splitter and cables. Additionally, these antenna arrays feature zero to 20° down tilt capability to compensate for the geography of the installation location. This helps ensure maximum wireless signal coverage in the service area.

 

 

Antenna Array Configurations Available

 

 

Antenna Arrays with four 90° sectorial antennas Antenna Arrays with four 90° sectorial antennas
Antenna Arrays with three 120° sectorial antennas Antenna Arrays with three 120° sectorial antennas
Antenna Arrays with two 180° sectorial antennas Antenna Arrays with two 180° sectorial antennas
 

All sectorized omni array configurations are designed to all-weather operation. They feature both heavy-duty polymer antenna radomes and stainless steel mounting systems. 

 
  
© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845