The More You Know: Fiber Terms 101

February 9, 2017 at 8:00 AM

 

They say knowledge is power, so we are here to empower you! The fiber terms 9/125, 50/125 and 62.5/125 might look like algebra to you, but here we’ll explain what they mean, how to read them and we even have a diagram and video to help enhance your educational experience.

 

The most common fiber cable sizes are 9/125, 50/125 and 62.5/125. These numbers refer to the diameter, in microns, of the core and cladding of a fiber optic cable. The leading numbers (9, 50 and 62.5) refer to the diameter of the fiber cable's core in microns. The trailing number (125) is the diameter (in microns) of the outside of the fiber cable's cladding. The cladding is a special coating that keeps the light from escaping the glass core of the cable. For quick reference, 9/125 is a single-mode fiber cable, 50/125 and 62.5/125 are multimode fiber cables.

 

Here is a diagram of the fiber core and cladding so you can see exactly what we’re talking about:

 

 

Click on the image below to watch our video that further explains the different fiber types.

 

Readers' Choice -Top Blog Posts of 2016

December 29, 2016 at 8:00 AM

 

As another year comes to a close, so does another chapter of our blog, Engineering Hub. We covered a wide variety of topics in order to keep you, our readers, in the loop with what’s going on in the world of wired and wireless technology. Here are highlights of the 2016 posts that were the most popular with our readers.

 


1.       802.11ay: 20 Gig Wireless!


The next generation wireless standard will blow you away with triple the speed and 30xs the transmission distance of 802.11ad. Learn about all of the benefits of 802.11ay and what it means for the world of wireless networking technology. (Read more)

 

 

 

2.       Fiber Showdown: Multimode vs. Single mode


Multimode and single mode are the two most common types of fiber optic cables. Both have very different attributes and one may work better than the other, depending on the needs of your application. This post will help you decide which will give you the best results. (Read more)

 

 

 

3.       Cat6 Cable: Shielded vs. Unshielded


Category 6 Ethernet cable is designed to provide high speed data rates, but how do you decide between shielded or unshielded? Here, we compare them side by side so you can choose which will work best for your application. (Read more)

 

 

 

4.       Good Vibrations: Vibration-Proof USB Connectors

 

Universal Serial Bus (USB) is one of the most widely used technologies to connect and power devices. One fundamental flaw of USB is its sensitivity to vibration, causing the connector to dislodge. In this post we show you some solutions to keeping your USB connected. (Read more)

 

 

 

5.      Next Generation Positioning: A look at what’s around the corner

 

GPS apps and positioning technology is something we use everyday to get directions or find something or someone nearby, and that usage is expected to continue to grow at a staggering rate. Here’s a look at what the IEEE has in store for next gen positioning technology. (Read more)

Fiber Showdown: Multimode vs. Single mode

February 4, 2016 at 8:00 AM

 

There are two main types of fiber optic cables, Multimode and Single mode. Depending on your application one might be better than the other to achieve optimal results. So how do you decide between Multimode or Single mode fiber optic cables? Let’s put these two side-by-side and see who comes out on top – a fiber Super Bowl, if you will.

   

Multimode

 

Single mode

 

  • ·       Large-diameter core which allows multiple modes of light to propagate
  • ·       High capacity and reliability
  • ·       Supports distances of up to 2km
  • ·       Less expensive
  • ·       Good for transmitting voice, video and  data signals over shorter distances 
  • ·       Mostly used for data and audio/visual applications in local-area networks and backbone applications within or between buildings (campus environments)
  • ·       Smaller core diameter which allows only one mode of light to propagate
  • ·       Much higher bandwidth
  • ·       Supports distances of 100km (optics dependant)
  • ·       More expensive
  • ·       Good for transmitting streaming voice, video and data over long distances
  • ·       Typically used in long-haul network links over extended areas by telecommunications companies and cable television networks

 

 

The optics used in fiber applications are not compatible and you cannot mix Multimode and Single mode fiber between two endpoints, so you must pick only one. What you choose really boils down to bandwidth, speed and distance.

 

Multimode will support a maximum bandwidth of 4700 MHz/km (OM4 laser optimized) and will extend to a distance of up to 2km (@100 Mbps). Currently the maximum speed supported on Multimode fiber is 100Gbps.

 

Single Mode fiber can support virtually unlimited modal bandwidth as well as Terabit data rates, it can also span up to 100km without the use of a repeater. Single mode cabling is being used heavily in large data centers and in long haul broadband carrier applications.

 

So your choice for fiber MVP will depend on the factors listed above and your specific application.

 

For a deeper look at the playbooks of these two cable types and to see a handy reference diagram, check out our blog post Fiber Fun Fact: Multimode vs. Single-mode.

 

How it Works: Fiber Optics

October 8, 2015 at 8:00 AM

 

Remember when you were a kid and would tie two tin cans together with a string to create a make-shift telephone?  Now imagine a high-tech version of that using pipe instead of a string, and if you shine a flashlight down that pipe it can be seen at the other end, despite curves and twists.  Turning the light on and off would allow you to communicate via Morse code.

 

Essentially, this is how fiber optic cables work, but they can carry millions of conversations and billions of bits of information per second!

 

Fiber optic cables use light pulses to transmit data from one end to the other. A coded beam of light is sent down a glass core that is surrounded by a mirror-like covering called cladding.

 

The cable’s core is made up of a thin strand of glass comparable to the thickness of a human hair. The glass is so pure that it allows light to shine through even though it may be several miles long.

 

The cladding covers the glass core to essentially create a mirror around the optical fiber and keeps the light contained.

 

Data transmissions made of light pass through the core, bouncing off of the cladding until it reaches the other end of the cable, where it is received and decoded by a fiber optic transceiver.

 

There are two types of glass fiber-optic cables: Single mode and Multimode.

 

Single mode is the simplest type of fiber optic cable.  Its core is small in diameter (typically 9 microns) and carries light signals straight down the middle of the fiber core without “bouncing” off the cladding. Single mode is ideal for longer distances and higher bandwidth applications. It can send information more than 100 kilometers before a repeater is necessary and is generally used in cable TV, internet and telephone applications.

 

Multimode fiber optic cable is larger in diameter (typically 50 or 62.5 microns). Its optical fibers are almost 10 times bigger than those in Single mode cable and allow light beams to travel through the core by following various paths. Multimode is used to send information over shorter distances. It is more economical, easier to work with and more common for Enterprise and SMB computer networks.

 

 No matter which type of fiber optic cable you choose, they all posses the following characteristics

 

·       Very low attenuation or loss over distance

·       Immunity to EMI and RFI

·       Hard to “tap” very secure

·       Very high bandwidth handling capabilities

 

Originally developed for medical use, fiber optic cables have revolutionized the telephone industry and have made internet accessible to the world. The possibilities for future applications are endless.

  

Explore our Fiber Optic product offering and check out our informative video that explains the different types of fiber optic cable.

 

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845