Case Study: HBM SoMat

March 8, 2018 at 8:00 AM

 

For more than 65 years, our customer HBM has provided precise and reliable products for a variety of test and measurement applications across a wide range of industries. HBM’s SoMat product line is an innovative portfoloio of precision data acquisition systems for field and lab analysis. Across industries including aerospace, automotive, oil and gas and everything in between, SoMat products  have helped companies by delivering rugged and modular data acquisition systems able to perform a range of on-board data processing while enduring harsh environments.

 

This issue HBM was having was finding a durable, custom interface cable solution at a competitive price for its SoMat product line. Their current cable did not provide the strain relief that was required by its customers. SoMat products used cables that had assembled backshells and because of the non-uniform shape of the cable bundle, the cables were pulling out of the backshell. This flaw was costing the company in product returns and repairs, and leaving customers unhappy.

 

L-com provided HBM with several custom engineered D-subminiature cable assemblies with molded backshells (similar to the one shown here) that were able to replace the existing assemblies. L-com’s cables solved the strain relief problem and reduced overall system cost without compromising design requirements, which fully met HBM’s customers’ requirements.

 

To read the full case study, click here.

 

Case Study: Kinki Sharyo

November 30, 2017 at 8:00 AM

 

In metropolitan areas, thousands of people depend on the rail system every day as a primary mode of transportation. Our customer, Kinki Sharyo, has designed and manufactured more than 10,000 railcars and is the leading supplier of low-floor light rail systems in North America. From manufacturing to maintenance, they design a full-range of customized products to meet the needs for each transit system to get people where they need to go safely and reliably.

 

After being awarded a $30 million contract from NJ Transit, Kinki Sharyo needed to make 60 new trains with DVI, Cat5e and USB cabling for onboard video and LED lighting systems. The problem they were having was finding a cable that could provide connectivity to articulated train cars that are connected to each other.  The existing connectivity method used heavy gauge cables bundled together that frequently wore out and had failure at friction points. They needed a robust cabling system that would not wear down and could withstand the movement of the train cars and constant flexing of the cables.

 

L-com provided Kinki Sharyo with crush-proof armored USB, right-angle Cat5e Ethernet and right-angle DVI cables all off-the-shelf and ready for installation. These cables met all the needs of the new rail car design. The USB cables were more than rugged enough, the right-angle DVI and Cat5e cables were the perfect fit for rail cars with limited space and they all provided the added benefit of low-smoke zero-halogen jackets to protect the new rail cars and passengers inside.

 

To read the full case study, click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845