Don’t Plan a WLAN Until You Read Our WiFi Antenna White Paper

April 3, 2014 at 10:00 AM

 

Why? Let me ask you this.

 

Do you know how to choose the correct antenna for a better wireless connection?

 

With all of the various antenna options out there, it can get confusing as to which antenna to use and how they work. After reading this white paper, you’ll have the information you need to get started on planning your network. 

 

Our white paper - Choosing the right WiFi antenna for your applicationcovers common wireless network application examples and details the basic types of WiFi antennas that are available today. From choosing an antenna for a campus, to planning for an office environment, we give you a rundown of what antenna is best for your application and how-to tips for proper network design.

 


Here are just a few highlights from this free white paper:

 


There are two main types of WiFi antennas, Omni directional and directional

 

Omni directional antennas provide a 360° donut shaped radiation pattern to provide the widest possible signal coverage in indoor and outdoor wireless applications. An analogy for the radiation pattern would be how an un-shaded incandescent light bulb illuminates a room. Types of omni directional antennas include "rubber duck" antennas often found on access points and routers, omni antennas found outdoors, and antenna arrays used on cellular towers. ... (read more)

 

Outdoor Omni Antenna

Rubber Duck Antenna

Omni Antenna Array

I want to add WiFi to my office building (inside)

 

To provide wireless coverage to an inside office space, use omni directional antennas that provide 360° wireless coverage. The style of antenna typically used is the ceiling mount omni directional antenna. The antenna gain pattern for the ... (read more)

 

 


I want to install WiFi in a campus environment (outside)

 

In this case you can use several directional antennas with an omni directional antenna at the central building to connect the buildings in the campus. This is called a point to multipoint network. As with any outdoor WiFi network, clear ... (read more)

 


 

to download this free white paper 

 

What is an Omni directional antenna for 2.4 GHz?

May 15, 2013 at 10:00 AM

 

Omnidirectional antenna

As wireless technology continues to grow and develop, several antenna shapes and designs have arisen to provide different types of coverage. An Omni directional antenna is so called because it provides a wireless signal in a 360° radius, or in "all directions". These types of antennas are very common, and typically look like a very straight, stick-like shape.

 

Since the energy of the signal is not directional or pointed in a specific way, Omni directional antennas tend to be of lower gain than directional antennas such as parabolic dish, Yagi, and panel style antennas. However, higher gain isn't usually required for small installations such as Wi-Fi "hotspots" in stores and cafes. For those kinds of applications, a single Omni directional antenna installed near the center of the location often does the trick.

 

The 2.4 GHz band is typically designated for Wi-Fi use, and is the most common band for things like laptop and tablet wireless access. Therefore, if you are setting up a network for customers or visitors to access the Internet wirelessly, you'll often be installing a 2.4 GHz antenna. However, check the specifications of the access point that is being hooked up to the antenna to make sure the frequencies match. 

 

Quick note: L-com has a huge selection of 2.4 GHz antennas, from parabolic dish antennas, to Omni directional and everything in between.
 
© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845