Why Use 802.3at PoE Technology?

April 17, 2014 at 10:00 AM

 

802.3at is the latest of the IEEE's Power over Ethernet (PoE) standards. Although it was released in 2009, it is still very relevant today.

 

Why? It offers up to 25-50 Watts of DC power to attached devices via a single Ethernet cable.

 

With the advent of 802.3at, a completely new class of devices could be powered directly via an Ethernet network interface. This PoE standard can be used with pan, tilt, and zoom (PTZ) IP cameras that require more power than stationary IP cameras, as well as other devices including dual radio WiFi access points, video phones, and laptops.

 

PoE enabled networking devices such as PoE IP Cameras, PoE Wireless Access Points and PoE IP Phones have become main stream in many networks because of the convenience of easy installation and great cost savings by not having to run AC power outlets.

Commonly referred to as PoE+ or PoE plus, 802.3at also has embedded intelligence via a newly defined data link layer (layer 2) protocol. The Link Layer Discovery Protocol (LLDP) allows the power source equipment to discover devices on the network and communicate with them to enable dynamic allocation of power levels.

 

PoE’s greatest benefit is that by utilizing its technology, both data and power can be sent to an Ethernet device via standard Cat5e/6 cabling. This means you do not need to install a power outlet at the device location and you can use readily available, relatively low cost Ethernet cabling.

If you’re looking to incorporate 802.3at technology into your application, here are a few products we suggest (all 802.3at compliant):

 

 

 

Understanding Copper/Fiber Media Converters

August 28, 2013 at 10:00 AM

What is a Media Converter?

 

Diagram of fiber optic premise wiring converted to copper with media converters

A media converter is used to extend Cat 5e/6 Ethernet cabling to distances beyond the 100 meter maximum for Ethernet by converting IP voice/video/data signals to fiber optic cabling.

 

Where are Media Converters used?

 

Media converters are used in environments where EMI/RFI is present, such as manufacturing facilities and other industrial environments. Other applications include campus networks where many buildings need to be connected via fiber. Also, high-rise buildings typically use a fiber backbone, which is laid vertically and taps into copper (UTP) networks on each floor via a media converter.

 

L-com's Media Converter offering

 

L-com offers media converters designed for both commercial and industrial use.

 

Commercial-grade fiber-to-copper media converters from L-com

 

L-com Ethernet Media Converter 10/100TX to 100FX MM SC 2km

- Plug-and-play installation
- Rugged metal case ensure longevity
- Multimode and Single-mode versions available
- Easy-to-read LEDs provide at-a-glance system status information
- Operating temp: 0°C to +70°C 

 

Industrial DIN Rail Media Converters from L-com

 

LCMC Media Converters

- 35mm DIN rail mounting
- Rugged aluminum case
- 24V DC power input
- Plug and play
- Operating temp: -40°C to +70°C

 

Tutorial on Wireless Networking

June 12, 2013 at 10:00 AM

 

Wireless network antenna and devices

Entire cities and even countries are looking into ways to expand communications access for their residents as the Internet has shifted from a luxury to an imperative. The most promising solution: wireless networking.

 

Why? Wireless networking allows a non-physical (well, at least non-cabled) connection to a wireless LAN (WLAN) and onto the World Wide Web for users. So what are you waiting for? Cut the cord!

 

Be mindful of this though- issues such as network and band congestion, security, signal range and propagation, power demands, and more make WLANs tricky to implement for all but the most informed network engineers and IT professionals. Yet there's no stopping this technology in its rapid advance, with solutions such as distributed antenna systems (DAS) and MESH networks beginning to show promise. For you to get started, here's a basic wireless tutorial on terminology and concepts.

 


Wireless Standards

 

Radio frequency signals can take a lot of different forms, so in order for devices made by different manufacturers to communicate, the IEEE has provided several standards including the mainstay for wireless Ethernet: 802.11.

 

The 802.11 standard specifies the band and IP protocol used to transmit data, and provides guidelines to maximize the speed of transmission. 802.11a, for instance, uses the 5Ghz band and can typically transmit at speeds up to 54 Mbps in shorter ranges. 802.11b, 802.11g, 802.11n, and the new 802.11ac all use various methods to increase the speed and range. The latest IEEE wireless standard, 802.11ac boasts transmission speeds of up to 1 Gbps!

 

Each standard typically requires wireless routers, access points, and other transmission equipment to match its designation, though there are many that can operate in multiple standards (such as routers that are 802.11b/g/n compliant).

 


Wireless Bands

 

In attempt to maintain order within the entire radio frequency spectrum that is available to us, the FCC and other global communications standardization organizations have designated or set aside specific ranges of frequencies for specific uses. We call these "ISM bands". ISM stands for industrial, scientific and medical to denote where these frequencies are used.  ISM bands (specifically the 2.4 GHz and 5 GHz frequencies) are also used in commercial wireless networks. 

 

Typically access points, antennas, and amplifiers all use either the 2.4 GHz band, 5.8 GHz band, or both for WiFi. Other ISM bands have been set aside for things like cell phone use, RFID chips, emergency/municipal use, and military use.

 


Wireless Security

 

As mentioned previously, one of the big emerging issues with wireless networking is security. Without a physical cable that can be plugged and unplugged, the only method to control who can do what on a network is to build it into the software and protocol. That means it is critical to set up a wireless network with appropriate security measures and to be aware of the security status of any network you connect to.

 

For most small networks, methods such as WPA, WPA2, or WPA-PSK allow the safe identification of nodes that should be allowed on a network with passwords and other controls. Wireless routers can also use access passwords to allow administrators to adjust or update security features as required.

 
If you have questions about a wireless project or application, contact L-com's technical support line for a live response and expert advice!
 
© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845