Hangin' Tough - Armored Cables

October 11, 2018 at 8:00 AM

 

When your cables need serious protection and the ability to stand up to the toughest conditions, an armored jacket might be the perfect solution. Armored cables are cables with a metal or plastic covering that provides a layer of protection that is much stronger than any traditional type of cable jacket. This suit of armor makes the cables extra tough and durable, now let’s take a look at just how tough they are.

 

The rugged characteristics of armored cables make them ideal for outdoor, industrial and military applications where these features are of the upmost importance. This includes factory automation, manufacturing and chemical and petroleum processing networks.

 

One of the biggest advantages of armored cables is there crush resistance rating. L-com’s metal armored cables offer a crush resistance of up to 1,500 PSI

which makes them well suited for just about any military or industrial application. Additionally these cables feature stainless steel armor that stands up to corrosion often found in extreme environments.

 

Plastic armor, although not as rugged as metal armor, offers an extra level of crush and abrasion resistance

when compared to non-armored cable jackets. L-com’s plastic armored cables feature a crush resistance of up 800PSI.

 

Even with all that armor, these cables are still capable of high speed transmission rates. Plus, they are offered in multiple varieties to suit a wide range of applications, including armored Ethernet, armored USB, armored HDMI, armored D-sub and armored DVI cable assemblies.

 

No doubt, armored cables are tough enough to withstand the abuse that might be faced in harsh environments and rugged conditions, and if you don’t believe us, watch this.

 

Video Blog- L-com's Toughest Cable Field Test

November 3, 2016 at 8:00 AM

 

Have you ever wanted to test your cables and really push them to the limit? If so, we have a video you MUST watch. We wanted to see just how much abuse our metal armored cables could endure, so we put them through our toughest test ever.

 

Our series of metal armored cables are capable of withstanding the harshest environments and are specifically designed for outdoor, industrial and military applications. Rugged metal armor protects the cable from damage and provides up to 1,500 pounds per square inch (PSI) of crush resistance. The metal jacket also secures the cable from dust, oil, moisture and UV damage. These cables can be used in a variety of industrial applications including factory automation, manufacturing and chemical or petroleum processing networks.

 

Our metal armored cables are currently available off-the-shelf in USB, DVI, HDMI, Ethernet (RJ45) and D-Subminiature styles. Plastic armored cable assemblies with up to 800 PSI of crush resistance are also available. In addition to our extensive off-the-shelf armored cable offering, we can also design and manufacture armored cables to your specifications.

 

Now, check out the video to watch our field test and see just how tough our armored cables are.

 

 

For more videos, tips and tutorials, click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845