Hangin' Tough - Armored Cables

October 11, 2018 at 8:00 AM

 

When your cables need serious protection and the ability to stand up to the toughest conditions, an armored jacket might be the perfect solution. Armored cables are cables with a metal or plastic covering that provides a layer of protection that is much stronger than any traditional type of cable jacket. This suit of armor makes the cables extra tough and durable, now let’s take a look at just how tough they are.

 

The rugged characteristics of armored cables make them ideal for outdoor, industrial and military applications where these features are of the upmost importance. This includes factory automation, manufacturing and chemical and petroleum processing networks.

 

One of the biggest advantages of armored cables is there crush resistance rating. L-com’s metal armored cables offer a crush resistance of up to 1,500 PSI

which makes them well suited for just about any military or industrial application. Additionally these cables feature stainless steel armor that stands up to corrosion often found in extreme environments.

 

Plastic armor, although not as rugged as metal armor, offers an extra level of crush and abrasion resistance

when compared to non-armored cable jackets. L-com’s plastic armored cables feature a crush resistance of up 800PSI.

 

Even with all that armor, these cables are still capable of high speed transmission rates. Plus, they are offered in multiple varieties to suit a wide range of applications, including armored Ethernet, armored USB, armored HDMI, armored D-sub and armored DVI cable assemblies.

 

No doubt, armored cables are tough enough to withstand the abuse that might be faced in harsh environments and rugged conditions, and if you don’t believe us, watch this.

 

Industrial Enclosures for any Application

October 4, 2018 at 8:00 AM

 

When it comes to protecting your valuable equipment, a NEMA enclosure can be a great solution. Whether your equipment could be exposed to the elements, chemicals, human tampering or theft, using an enclosure can ensure your investment is protected and provide you with peace of mind. Different enclosures provide different benefits, and you must find the best fit for your application. Here, we’ll take a closer look at Industrial enclosures and all that they have to offer.

 

When it comes to location, industrial enclosures can be used for both indoor and outdoor applications. In any setting, industrial enclosures provide extra security against theft, tampering and damage. Standard enclosures are lockable and keyed locks can be added as an extra measure to keep valuable components safe. Weatherproof outdoor enclosures can provide superior protection from the elements for outdoor wireless access points and sensitive electric components. Plus, with the option of adding heating and cooling or power, these enclosures deliver dependable performance in any climate.

 

There are numerous features that make industrial enclosures ideal for protecting sensitive equipment, these include mounting plates that securely mount equipment inside an enclosure and a thermostat controlled cooling fan that keeps equipment cool in high temperature environments. Also, a mounting lid can prevent damage and theft of the equipment inside the enclosure, these lids can have hinges, removable lids or clear viewing windows for easier viewing while maintaining security. Power over Ethernet (PoE) interface is another great feature that delivers power to the enclosed equipment where power sources are limited, plus it provides additional surge protection for internal PoE compatible equipment.

 

Many applications can benefit from the use of an industrial enclosure, and while the details might vary, they all share a similar set of requirements that include being able to operate under exceedingly harsh conditions that include exposure to corrosive chemicals, extreme temperatures and more. Some of these applications include industrial automation, oil and gas, and transportation. Rugged, industrial enclosures are also ideal for security and automation applications such as access controls, fire alarms, video surveillance equipment and building automation.  Indoor and outdoor enclosures can be used in a variety of locations to protect equipment, including cell towers and rooftops, open-access basements, telecom closets, shopping centers and factories.

 

Overall, industrial enclosures are a great way to keep expensive equipment safe. In almost any application, and even in the harshest conditions, they provide a level of security that is unmatched. To take a look at L-com’s complete, comprehensive line of industrial enclosures, click here.

 

Video Blog- L-com's Toughest Cable Field Test

November 3, 2016 at 8:00 AM

 

Have you ever wanted to test your cables and really push them to the limit? If so, we have a video you MUST watch. We wanted to see just how much abuse our metal armored cables could endure, so we put them through our toughest test ever.

 

Our series of metal armored cables are capable of withstanding the harshest environments and are specifically designed for outdoor, industrial and military applications. Rugged metal armor protects the cable from damage and provides up to 1,500 pounds per square inch (PSI) of crush resistance. The metal jacket also secures the cable from dust, oil, moisture and UV damage. These cables can be used in a variety of industrial applications including factory automation, manufacturing and chemical or petroleum processing networks.

 

Our metal armored cables are currently available off-the-shelf in USB, DVI, HDMI, Ethernet (RJ45) and D-Subminiature styles. Plastic armored cable assemblies with up to 800 PSI of crush resistance are also available. In addition to our extensive off-the-shelf armored cable offering, we can also design and manufacture armored cables to your specifications.

 

Now, check out the video to watch our field test and see just how tough our armored cables are.

 

 

For more videos, tips and tutorials, click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845