The Ultimate List of Fiber Cable Connectors and Colors

June 5, 2014 at 10:00 AM

 

You can practically see the rainbow when you look at our fiber cable offering on our website or in our catalog. 

 

In the world of fiber optics, there’s a standard color scheme to identify each and every type of fiber cable.  

 

And then there are all of those connectors to choose from… ST, SC, LC, MTRJ…

 

Though you may have heard of them, it can be challenging to identify the difference between each type of connector. 

 

We’re here to break it down. In the following tutorial, we’ll highlight some of the most common colors and connector types that you should be aware of. 

 

If you’re going to deploy a new network system using fiber or would like to better organize your existing fiber cables, you’ll want to stick around.

 


COLORS

 

So what do they all mean?

 

Traditionally, the following jacket colors have been used to define Single mode and Multimode fiber cables:

 

Yellow

9/125 Single mode

 

Orange

50/125 Multimode

 

Aqua

50/125 
(10 Gigabit Optimized)

 

Slate (Gray)

62.5/125 Multimode

 

 
 
 
 

Over time, the use of fiber has expanded in many applications and the need for different jacket colors has become a requirement for some customers. In today’s telecommunications networks you might also see different jacket colors used to denote different services or devices.

 

For example, if you have already allocated your traditional orange 50/125 cables to all of your high speed server connections, you can now add blue 50/125 fiber cables to denote WAN router connections.

 

By using colors to identify services/devices, troubleshooting is made easier, thereby decreasing network downtime. 

 

L-com has also developed a line of red, blue, green and yellow jacketed fiber cables which make port and service locations easier to find in dense equipment racks. 

 
 
 

       

 

 



CONNECTORS

 

In addition to the range of cable jacket colors, you can choose from an extensive variety of Fiber Optic connector types

 

The most common connector types you’ll see are: LC, SC, MPO and ST style connectors.

 

All of these types of connectors can be used with either Multimode of Single-mode fiber.

 

There are three types of polishes which can be applied to a fiber connector: PC or Physical contact, UPC or Ultra Physical contact and APC or Angled Physical contact.

 

Each polish type exhibits a different level of back reflection. Back reflection is a measure of the light reflected off the end of a fiber connector. This light is measured in decibels. For certain applications, the amount of back reflection on a fiber connector is critical.

 

L-com’s fiber connectors include commercial grade field installable fiber optic connectors as well as rugged IP67 fiber connectors for use in harsh environment applications.

 

In addition to our fiber connector video, check out one of the most popular technical resources we have- our Fiber Optic Connector Chart- that can help you find the fiber connector you’re looking for.

 


WAIT, THERE’S MORE…

 

In addition to standard commercial and industrial connectors, there are also Keyed LC Singlemode 9/125 assemblies which have a variety of COLORED CONNECTORS.

 

L-com's Keyed LC line of Fiber Optic Cable Assemblies offers mechanical network security for organizations desiring to segregate networks due to privacy or security concerns. Each Keyed LC connector is color coded for identification and features a mechanical key which prevents users from accidentally connecting the cable to the wrong jack. 

 

There are a total of 12 colors available including: Brown, Cobalt, Gray, Magenta, Olive, Orange, Pink, Red, Turquoise, Violet, White and Yellow. These cables are OFNR rated to meet strict building codes and utilize Single mode 9/125 fiber. Match the color of the Keyed connector to the corresponding color of Keyed coupler to create a secure network connection. 

 

Do your eyes hurt yet?

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845