Embedded Antennas and the IoT

May 2, 2019 at 8:00 AM

 

In the not so distant future, the world will be fully automated with machines being able to communicate with little or no interaction from humans, thanks to the arrival of the Internet of Things (IoT) and the use of embedded antennas.

 

These small form factor antennas are a perfect fit for the shrinking size of IoT devices, while still being able to keep up with the massive amounts of data that will need to be transmitted as the IoT connects physical devices with software based management and control applications.

 

Embedded antennas are small, yet powerful antennas with many offering multiband support for use in mobile and fixed data applications. Their key performance attributes include high efficiency, low power consumption, low return loss and isolation.

 

High efficiency brings better signal reception, improving the system’s ability for faster data transfer rates. Reduced power consumption allows for increased longevity. Less return loss means more power transmitted, and isolation limits the amount of crosstalk interference. Embedded antennas can work with high-frequency or low-frequency systems, some feature MIMO technology and smart antennas have been introduced that feature embedded GPS and Flash memory capabilities.

 

As IoT deployments get underway, there are more embedded antenna options to consider to take full advantage of this exciting era of automation.

 

To help you succeed with your IoT implementations, we offer a full line off-the-shelf, embedded antennas ready to ship the same-day, plus custom designed antennas to suite all of your IoT needs.

 

Antennas & the IoT

January 11, 2018 at 8:00 AM

 

With all the excitement surrounding the development of the IoT, there is one important part that can’t be overlooked – the antenna. Antennas are integral to implementation of the IoT. Connecting all of the physical objects that make up the IoT requires antennas transmitting a massive amount of data. Thus, without antennas, there would be no IoT.

 

As IoT use increases, so does the demand for more antennas that meet the needs of IoT applications and meet the expectations of users. Thus, antenna manufacturers and designers have had a voice in the development of IoT devices and are meeting the call for antennas that are up to the task.

 

Here are some of the ideal traits for antennas designed for IoT applications:

 

Small Form Factor – One of the biggest trends in IoT antennas is smaller form factors. As IoT devices are being implemented in more industries, manufacturers are looking to shrink device footprint. And as devices get smaller, so must the antennas. These small form factor antennas include embedded antennas, PCB antennas and chip antennas.

 
High-Performance – Designers have been working to deliver small antennas without sacrificing performance capabilities because demand for speed and capacity is also growing. Even if the device is the size of a coin, its antenna still needs to meet high-performance standards.
 
Cost-Effective – Adding antennas onto all of these devices can be costly. As device demand increases, manufacturers have begun looking for antennas that will be economic to use on the devices. 
 
Beyond being small, powerful and cost-effective, there are some other areas of antenna technology that are emerging with the development of the IoT. These include:
 
Two antennas – While two antennas will not be necessary for MIMO communications with lower category LTE devices, two antennas will be needed for Cat4 and above in order to meet requirements for higher speed and throughput systems. LTE cellular networks will also continue to use two cellular antennas to fully achieve high-speed performance.
 
MU-MIMO – Multi-User Multiple-Input Multiple-Output (MU-MIMO) has breathed new life into Wi-Fi by allowing multiple devices to communicate with the access point at the same time. This has made a significant improvement to wireless network throughput and impacted dense, high-capacity networks.
 
Low-Power – Low-power technologies, such as ISM-band solutions, are being developed to provide longer battery life for devices and allow long-range communications at a low-bit rate. Plus, smartphone technologies such as Bluetooth Low-Energy (BLE) are being adapted to be utilized in IoT applications.
 

Antennas & the IoT

January 11, 2017 at 8:00 AM

 

With all the excitement surrounding the development of the IoT, there is one important part that can’t be overlooked – the antenna. Antennas are integral to implementation of the IoT. Connecting all of the physical objects that make up the IoT requires antennas transmitting a massive amount of data. Thus, without antennas, there would be no IoT.

 

As IoT use increases, so does the demand for more antennas that meet the needs of IoT applications and meet the expectations of users. Thus, antenna manufacturers and designers have had a voice in the development of IoT devices and are meeting the call for antennas that are up to the task.

 

Here are some of the ideal traits for antennas designed for IoT applications:

 

·       Small Form Factor - One of the biggest trends in IoT antennas is smaller form factors. As IoT devices are being implemented in more industries, manufacturers are looking to shrink device footprint. And as devices get smaller, so must the antennas. These small form factor antennas include embedded antennas, PCB antennas and chip antennas.

 

·       High-Performance - Designers have been working to deliver small antennas without sacrificing performance capabilities because demand for speed and capacity is also growing. Even if the device is the size of a coin, its antenna still needs to meet high-performance standards.

 

·       Cost-Effective – Adding antennas onto all of these devices can be costly. As device demand increases, manufacturers have begun looking for antennas that will be economic to use on the devices.  

 

Beyond being small, powerful and cost-effective, there are some other areas of antenna technology that are emerging with the development of the IoT. These include:

 

·       Two antennas – While two antennas will not be necessary for MIMO communications with lower category LTE devices, two antennas will be needed for Cat4 and above in order to meet requirements for higher speed and throughput systems. LTE cellular networks will also continue to use two cellular antennas to fully achieve high-speed performance.

 

·       MU-MIMO – Multi-User Multiple-Input Multiple-Output (MU-MIMO) has breathed new life into Wi-Fi by allowing multiple devices to communicate with the access point at the same time. This has made a significant improvement to wireless network throughput and impacted dense, high-capacity networks.

 

·       Low-Power – Low-power technologies, such as ISM-band solutions, are being developed to provide longer battery life for devices and allow long-range communications at a low-bit rate. Plus, smartphone technologies such as Bluetooth Low-Energy (BLE) are being adapted to be utilized in IoT applications.

 

Embedded Antennas Connecting our World

October 22, 2015 at 8:00 AM

 

Imagine a world where machines communicate without human involvement. Now take that a step further and picture a world that is fully automated. With the development of the Internet of Things (IoT), this world could become a reality.

 

The IoT is a network of physical objects embedded with technology that will offer advanced connectivity and a seamless exchange of data with little or no human interaction. 

 

How is all of this going to be possible? With the adoption of the IoT comes the development of advanced mobility technologies and the integration of embedded antenna technology. 

 

Embedded antennas are small, yet powerful with multiband systems used for mobile voice, video and data applications.

 

Embedded antennas’ key performance attributes include high efficiency, low power consumption, low return loss and isolation.

 

High efficiency brings better signal reception, which improves the system’s ability for faster data transfer rates. Reduced power consumption allows for increased mobility. Less return loss means more power transmitted, and isolation limits the amount of crosstalk interference.

 

Embedded antennas can work with high-frequency or low-frequency systems, some feature MIMO technology and smart antennas have been introduced that feature embedded GPS and Flash memory capabilities.

 

IoT is expected to exceed machine-to-machine communications and usher in global automation that will encompass both personal and business applications.  It is also expected to produce large amounts of data to be collected at extremely high speeds. With all of these things connecting to one another, embedded antennas will play a key role in the future of IoT applications.

 

 

  

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845