How Network Security is Changing

November 29, 2018 at 8:00 AM

 

With more users providing more information on more networks, and some of those networks being breached, it’s no wonder that network security is a hot topic for many people and businesses. In fact, network security is a top concern for many IT administrators. For, as network technology has become more advanced, so have the ways in which those networks can be hacked. Here, we’ll take a look some of the changes happening in network security to counteract those threats.

 

·        Network security will no longer be a small branch of IT, but rather a responsibility that encompasses the entire organization. The network is a part of every aspect of IT and thus it will need to be protected by all administrators. Plus, the network itself should be armed with tools to help avoid attacks by reinforcing network-based security such as firewalls and malware prevention.  

 

·        Today, so many things are being sent to the Cloud, and so will security. Many IT departments will take advantage of cloud-based services that will manage common security tasks as part of a contracted agreement. This allows a simple subscription plan to impart dynamic security measures that once took several hours for administrators to manage. Multi-Cloud security management platforms will also come into play to allow network security to be managed across public and private clouds via a single security control plane.

 

·        We’ve all seen the IT email alert go out warning of an email scam sent to employees to get them to click a link that then installs malware on the network. Because of these types of attacks, end-point security has become a priority. This has extended to include mobile device management for non-corporate owned devices. In the future, many of these end-point security measures will be simplified and condense the number of protection tools in place to provide better overall protection.

 

·        Penetration (pen) testing is a valuable tool used to detect security gaps that might not have been identified by IT staff. Outside firms are often hired to perform this testing for a true outside party perspective, but the service can be costly and needs to be done in a timely manner. With the development of new AI and automation technology, pen testing is becoming easier and less expensive, meaning that it can be done more often, which is especially beneficial to keep up with the increase of new viruses, malware and other cyber threats.

  

With these upgrades in network security, along with an increased focus on overarching enterprise wide security procedures, today’s networks will be able to keep up with tomorrow’s technology and do it securely.

 

Smart Homes - The Future is Here

September 20, 2018 at 10:00 AM

 

Long ago, the idea of a home having the technology to be interactive was only a possibility in a Hollywood production or sci-fi novel. But those days are gone, the future is here and smart homes have moved from the realm of fantasy to an endless world of possibility. With the development of the Internet of Things (IoT), the world in general is becoming smarter and safer, and that includes our homes. Here, we’ll take a look at the technology behind the innovation bringing technological magic to your home.

 

First, what is a smart home? A smart home is automated, much in the way your coffee pot or your air conditioner are automated to turn on at a certain time or temperature. But a smart home takes that one step further by connecting all of those automated devices in your home through a wireless network, they are then able to be monitoring and programmed from one device. It is that communication with the devices that makes it smart. The devices in a smart home all rely on connectors and sensors to transmit and relay signals. Most wireless home automation uses low-power equipment so that power supply is not an issue.

 

To connect all of these devices, a combination of long and short-range wireless communication protocols is used, such as Wi-Fi, Bluetooth, ANT and ZigBee. With this technology, along with smartphones and tablets, we are now able to connect a multitude of devices within the home, this includes TVs, heating and cooling systems, lighting, appliances, security systems and cameras, or anything else that can be connected to the network. Plus, the communication to these devices is not distance limited, meaning you can control or change your thermostat while you’re at work or traveling using WAN connectivity via a router. Many new homes are being constructed with this technology built-in, older homes can be retrofitted with smart technologies and there are devices from companies like Google and Amazon that will connect to many electronics within your home.

 

Why would someone want a smart home? For one, it can make life a lot easier. Being able to control the devices within your home from your smartphone is super convenient. There is also an additional level of safety added when you’re able to monitor your home through a connected security network. Video cameras can provide surveillance in and around the home, with smart locks you can allow repairmen into your home and you are able to monitor when children get home from school. For people with disabilities or limited movement, smart homes that allow them to manage the home environment from a single, mobile device can make life much easier. In addition to safety, smart homes can be very energy efficient, which is good for the environment. Being able to control the thermostat remotely and turn lights and appliances on or off can be a great way to save energy.

 

With the growth of the IoT and more things becoming connected, it is no wonder that this would apply to our homes as well. Not only do smart homes provide convenience, they can also be good for the environment and give assistance to the disabled. Lucky for us, we no longer have to wait for the home of the future, the future is now. 

 

5 Technologies Changing the World

March 23, 2018 at 10:00 AM

 

In this age of technological advancement, the world is changing faster than ever. In fact, it’s hard to find an industry or area of our lives that hasn’t been touched by some type of technology. Here, we’ll take a look at some of the biggest technological advancements that are changing the world around us.

 

Clean Energy

 

As more data is showing that the Earth is getting warmer, there is more attention being paid to clean energy as a real solution. In the past, attempts to combat climate change by implementing clean energy has been a hard sell. But scientists, engineers and entrepreneurs have been hard at work creating new options that make clean energy convenient and cost-effective. Since 1977, the price of solar cells has dropped 99.5% as a result of technological and manufacturing advances in clean energy. At this rate, it’s possible that solar will soon cost less than fossil fuels. The cost of wind energy has also dropped dramatically and represents one-third of newly installed US energy capacity in the last decade. Wired and wireless networks are being built to support the energy industry as more countries and organizations are taking advantage these cost savings and moving towards clean energy, a trend that could have a big impact on the world.

 

Computerized Medicine


The role of wired and wireless technology and computers in medicine is expanding from record keeping to applied technologies that are leading to medical breakthroughs. Data analysis software is analyzing genetic sequencing to detect things like cancer and help determine the best course of treatment. Technology is aiding in huge advancements in prosthetic limbs and brain-to-machine interfaces will soon allow prosthetics to be controlled by our thoughts. Computers are also becoming more proficient at diagnosing diseases. Recently, an artificial intelligence system used patterns in 20 million cancer records to make a diagnosis that doctors weren’t able to make. Furthermore, it is expected that in 10-15 years we will be able to reverse paralysis with brain implants that will restore movement taken away by spinal cord injuries.  

 

3D Printing

 

There is a lot to like about 3D printers, they open up a new world of possibilities. 3D printers allow designers, engineers or consumers to take a design directly from their computer and make it into a physical object. From creating product parts without the cost of tooling, to prosthetic limbs, toys and even food, the possibilities of a 3D printer span as far as the imagination can dream. And with the price of 3D printers dropping dramatically, those possibilities will be open to more and more people, creating an expanded realm of innovation like we’ve never seen before.

 

Self-Driving Vehicles

 

Over the next 2-4 years, self-driving cars are expected to become a mainstream mode of transportation and reshape the world. There are already self-driving cars on the road that are safer than human-driven cars in most conditions. With cars being the leading cause of death for people ages 15-29 years old, a safer car could save a lot of lives.  Most self-driving cars will be used continuously through a ride-hailing app, Lyft is using them already in Boston. This would drastically reduce the need for parking spaces which take up 20-30% of usable space in most cities. Furthermore, the idea of cars communicating with one another to avoid accidents and alleviate traffic jams, all while allowing human riders to spend commuting time interacting with one another, working or studying, will truly be revolutionary.

 

Artificial Intelligence and Automation


Most people have had an experience with an automation in the form of an automated customer service system when calling a company or office. Those types of systems, which can be very frustrating at times, are going to become more prevalent. Fortunately, they’re also going to get much better. Smart devices will also be able to make better, more accurate suggestions and recommendations by learning humans’ patterns and preferences with increased automation. We are likely to see more automation and artificial intelligence (AI) infiltrating more and more industries. From manufacturing to fast food to journalism, more jobs will become fully or partially automated. We could see self-serve food kiosks in the near future and automated drones are already being tested to make deliveries. With all of these technological advancements comes a fear of lack of interpersonal communication, but hopefully with more services being automated, humans will take advantage of having more time to interact with one another.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845