Wizarding World of Our Product Wizards

June 14, 2018 at 8:00 AM

 

Have you ever felt overwhelmed while trying to find the right parts for your application? Ever felt lost in a world full of connector, cable, antenna, adapter and amplifier options? Have you ever dreamed of being able to find exactly the product you need with the click of a mouse or touch of the screen.  Fortunately, you don’t need a magic wand for your wish to come true, our product wizards are here to help with no magical powers necessary.  

 

We have designed 18 product wizards that, just like magic, are able to determine the exact product you need. With minimal input from you, these wizards can help you navigate through a plethora of product options, taking the guesswork out of finding what’s right for your application.

 

Our product wizards are simple and easy to use. For example, to determine the perfect antenna for your application, our antenna product wizard only has 4 questions before showing you all of your antenna options:

 

1.      Select antenna frequency

 

2.      Choose type of antenna

 

 

3.      Pick antenna gain

 

 

4.      Select antenna connector

 

5.      Then behold the magic of the product wizard

 

 

Here is list of our product wizard available to use anytime and free of charge:

 

·        Adapters

·        Amplifiers

·        Antennas

·        Cable Assemblies

·        Coax Lightning Protectors

·        Connectors

·        Ethernet Converters

·        Hubs or Switches

·        KVM Switches

·        Lightning Protectors

·        Network Interface Cards

·        Rack Panels

·        Signal Filters

·        Signal Splitters

·        Switch Boxes

·        Tools

·        Weatherproof Enclosures

·        Wireless Adapters

 

No matter what your application is, our product wizards have the power to make your product search much easier and provide you with exact results in a flash.

 

Case Study: Lineage Logistics

May 10, 2018 at 8:00 AM

 

As the second largest cold storage thrid-party provider in the US, Lineage Logistics provides cold storage solutions for leading grocery, food and retail  companies.

 

During a wireless network roll-out in their warehouses, Lineage Logistics needed to add multiple access points inside refrigeration units with temperatures as low as -40 degrees. The company’s engineers had designed a wireless access point that fulfilled the needs of the project, but wasn’t able to function unprotected in the cold temperatures.

 

Lineage Logistics began searching for an enclosure that would protect their access point, offer Power over Ethernet (PoE) over a single cable and meet cost requirements.

 

After rejecting a competitor’s offering, as it didn’t fully meet the requirements, Lineage Logistics came to L-com for help. Our team was able to develop a comprehensive solution that met all their needs. We created a custom NEMA enclosure that could house the access point and provide plently of room if adjustments were needed. We were also able to save Lineage Logistics time and money on installation by mounting the access points in the enclosures and providing all required cabling and antennas.

  

L-com was able to not only meet, but surpass this client’s expectations with the perfect solution to their problem.

 

To read the full case study, click here.

 

How Tech is Changing Transportation

April 19, 2018 at 8:00 AM

 

These days, it’s hard to find a part of our everyday lives that’s not being transformed in some way by technology. Transportation is no different. Driverless cars have been at the forefront of most transportation technology discussions lately, but do you know other ways that tech is changing how we get from point A to point B? Here, we’ll take a look at some of the ways technology is changing the transportation industry.

 

Rail

 

Railways are one of the oldest forms of transportation still used today. At their inception, trains were a groundbreaking way for people to get back and forth for everyday commutes, to explore places they’d never been and to transport goods at speeds that were unheard of at the time. Rail systems are still used today for many of the same reasons, but they are much smarter. Today’s rail yards have wired and wireless technology that allows for communication throughout the rail yard to provide security, control and real-time data collection.

 

RFID technology has also been put in place to modernize asset management in rail yard operations. Instead of employees walking from one car to another, manually recording inventory, today’s systems use electronic scanners to record asset information accurately and without the variable of human error. This data is then sent back to a central office where assets can be monitored in real time.

 

Technology is also being used to make rail travel safer by using wayside monitoring applications to record real-time data such as speed, time of passing and track conditions. This critical information is used for real-time scheduling and to generate safety alerts.

 

Roadways

 

Until all of those self-driving cars get on the road, and possibly still after, making roadways safer is another way technology is affecting the transportation industry. In tunnels, cellular and Wi-Fi service are provided by antennas while IP cameras connect to an Ethernet network. These cameras provide real time surveillance to a tunnel control center, so traffic and safety concerns can be monitored live. Digital signs are also connected to the Ethernet network, allowing them to be controlled remotely.

 

Intelligent Transportation Systems (ITS) use wired and wireless technology to control roadway traffic signals and vehicle and pedestrian safety systems. These systems utilize technology to manage traffic flow and ease congestion on the roads. Roadway security and overall safety is also improved with IP cameras and traffic sensors providing live surveillance and control.

 

With the use of wireless technology, roadside digital signs are able to deliver real time messaging along roadways with live updates being delivered from a central control office. These messages can include weather updates, traffic and road condition alerts and information on alternate routes, all of which can make travel easier, more efficient and save lives.

 

Maritime

 

An entire ship, including every part of shipboard communications and surveillance, can be managed via a central management station by using an Ethernet network and Simple Network Management Protocol (SNMP). 

 

IP cameras are used for monitoring, cables connect propulsion and steering systems to a controller, and antennas allow for voice and data communications and RFID management of cargo containers.

 

To load and unload ships, modern seaport terminals use automated crane systems to save freight companies millions of dollars in labor, maintenance and repairs. Computers are housed in a secure location, connected to Ethernet networks and used to control the cranes. This wireless network allows remote control over operations without the cost of running cables.

 

On the dock, keeping track of personnel, assets and ground support vehicles is made easier with wireless communications. Antennas allow for communication with the central operations command center. They also support Intermodal container RFID tracking systems which enable wireless devices to quickly and accurately process container and inventory information in real-time. With cellular and Wi-Fi communication between crews, freight companies can save money and increase security by eliminating the need for traditional radio communications.

 

For an in-depth look at what L-com products are being used to deliver technology to the transportation industry, click here.

 

Connectivity Solutions for Every Application

May 7, 2015 at 10:00 AM


Did you know L-com not only manufactures a wide range of cables, adapters, connectors and other wired products, but we also design and manufacture a slew of wireless networking gear including antennas, amps, RF splitters and filters and more!

 

If you didn’t know, L-com is an established global leader in the manufacture of wired and wireless connectivity products, offering a vast array of solutions for just about every industry imaginable.

 

From POS credit card scanning systems to fighter jet flight control systems, L-com’s products can be found all over the world and in many different applications.

 

Our mission is to provide you with the product(s) you need where and when you want them. This includes custom solutions when an off-the shelf option just can’t get the job done.

 

We have over 30 years of experience designing and building custom connectivity products. With a global presence including manufacturing and support locations from the United States to China, we can provide custom connectivity products designed to your specifications.  

 

Take a look below to see some of our most popular off-the-shelf product categories and if you can’t find what you need at www.l-com.com please contact us to see how we can help you with you custom product request.

 

Antennas

Cable Assemblies

Connectors

Adapters

 

4.9-5.8 GHz 22 dBi Broadband Weatherproof Grid Antennas

Cat5e Shielded Ethernet Cable- 26 AWG Stranded PVC Industrial Ethernet Patch Cords - Blue

http://www.l-com.com/product_images/detail/PWD_ABM-1704.JPG

USB Surge Protector - Panel Mountable and with or without Pigtail Cable

 

Don’t Plan a WLAN Until You Read Our WiFi Antenna White Paper

April 3, 2014 at 10:00 AM

 

Why? Let me ask you this.

 

Do you know how to choose the correct antenna for a better wireless connection?

 

With all of the various antenna options out there, it can get confusing as to which antenna to use and how they work. After reading this white paper, you’ll have the information you need to get started on planning your network. 

 

Our white paper - Choosing the right WiFi antenna for your applicationcovers common wireless network application examples and details the basic types of WiFi antennas that are available today. From choosing an antenna for a campus, to planning for an office environment, we give you a rundown of what antenna is best for your application and how-to tips for proper network design.

 


Here are just a few highlights from this free white paper:

 


There are two main types of WiFi antennas, Omni directional and directional

 

Omni directional antennas provide a 360° donut shaped radiation pattern to provide the widest possible signal coverage in indoor and outdoor wireless applications. An analogy for the radiation pattern would be how an un-shaded incandescent light bulb illuminates a room. Types of omni directional antennas include "rubber duck" antennas often found on access points and routers, omni antennas found outdoors, and antenna arrays used on cellular towers. ... (read more)

 

Outdoor Omni Antenna

Rubber Duck Antenna

Omni Antenna Array

I want to add WiFi to my office building (inside)

 

To provide wireless coverage to an inside office space, use omni directional antennas that provide 360° wireless coverage. The style of antenna typically used is the ceiling mount omni directional antenna. The antenna gain pattern for the ... (read more)

 

 


I want to install WiFi in a campus environment (outside)

 

In this case you can use several directional antennas with an omni directional antenna at the central building to connect the buildings in the campus. This is called a point to multipoint network. As with any outdoor WiFi network, clear ... (read more)

 


 

to download this free white paper 

 
© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845