802.11ad - What is WiGig?

November 15, 2018 at 8:00 AM

 

As the evolution of wireless technology continues, so does the development of new wireless standards. Next on the list is 802.11ad – also known as WiGig. Most of the emerging wireless standards have been a steady progression, but this one has some fundamental changes planned. Here, we’ll explore what WiGig is all about.

 

As far as speed is considered, WiGig will support data rates up to 7 Gbps, though real data rates might be less than this maximum limit. WiGig operates on the 60 GHz frequency, as opposed to Wi-Fi which uses the 2.4 to 5 GHz bands. This should result in much less congestion compared to Wi-Fi’s congested frequencies and WiGig also shouldn’t have as many interference issues as there are on the 2.4 GHz Wi-Fi band. Plus, it utilizes a narrow signal beam to reduce attenuation. But with a range of only around 30 feet and the 60 GHz signal unable to penetrate obstacles, WiGig is limited to one room with a clear line of sight from the transmitter to the receiver.

 

Instead of MIMO, WiGig uses multiple antennas for beamforming, which helps reduce attenuation. WiGig beamforming utilizes a phased antenna array that provides a signal power boost in whichever direction it is aimed. One of these access points can have as many as 64 antennas to generate up to 128 beams.

 

For multiple access, Service Period (SP), a new channel access mode, has been added to WiGig. This creates transmission schedules that are assigned to clients by access points. Time on the channel is organized into intervals called Beacon Intervals (BI). SP access is projected to be the preferred channel access in WiGig.

 

WiGig will also introduce a new mode of operation called PBSS. With PBSS, there is a central coordinator, like an access point (AP), but it allows clients to communicate while surpassing the AP. Clients can also talk to one another directly with this. PBSS is designed for applications that stream HD video to a display, because it doesn’t require the video to be sent through the AP, but it can still connect through the AP in other areas of the network.

 

In addition to 2.4 and 5 GHz, future Wi-Fi devices are expected to include 60 GHz radios and are expected to be capable of seamless transfers between the bands. Not only is WiGig bringing something new to today’s wireless networks, but it will add extra capability to future applications.

 

802.11ay: 20Gig Wireless!

March 31, 2016 at 8:00 AM

 

Hold on to your hats – or in this case, your wireless devices – and prepare to be blown away by 802.11ay. The next generation wireless standard promises almost three times the speed of 802.11ad with transmission rates of 20 Gbps, up from 802.11ad’s current rate of  7 Gbps. It will also extend transmission distance from the 10 meter limit of 802.11ad to as far as 300-500 meters!

 

Scheduled for release next year, 802.11ay will increase bandwidth and improve the reliability and robustness of the 60GHz millimeter wave spectrum. It will be designed to improve throughput, range and use-cases.

 

The focus of 802.11ay will be on new applications for mobile offloading, wireless docking and display as well as indoor and outdoor wireless backhaul. It is also expected to include mechanisms for MU-MIMO and channel bonding technologies.

 

The main targets for 802.11ay are DisplayPort, HDMI and USB connectivity, fast synch as well as short-range, high-bandwidth connectivity to TV and monitor displays.  

 

As an amendment for improving the performance of the 802.11ad standard, 802.11ay will support the same broad applications and be backward compatible with the 802.11ad standard.

 

802.11ay is primed to pack a punch with super-charged 20 Gig speeds and greater transmission distance. This revolutionary IEEE standard will surely break records and set the standard for future wireless technology.

 

Posted in: Wireless

Tags: , , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845