All About USB 3.2

January 10, 2019 at 8:00 AM

 

We’ve discussed the difference between USB 3.1 Gen 1 vs. Gen 2, but now comes the next level for Universal Serial Bus - USB 3.2. What makes this newest USB standard stand out? First and foremost are increased bandwidth and USB Type-C connector and cable support. Here, we’ll take a look at all the specs, so you’ll know all about USB 3.2.

 

While USB 3.1 Gen 1 brought 5 Gbps and Gen 2 doubled that to 10 Gbps speeds, USB 3.2 then doubles down again to offer 20 Gbps speeds – the most notable feature of the new standard. The way it provides those speeds is a little different though. USB 3.2 utilizes what is being called multi-lane operation, where devices use two lanes of 5 Gbps or 10 Gbps running together to transfer data at the same time over extra wires inside the USB cables. This allows for a cumulative data transfer rate of 10 Gbps to 20 Gbps.

 

What does this new standard mean for older USB cables? Fortunately, the new standard will be backward compatible with older standards. Even more fortunately, if the host and recipient devices are USB 3.2 compatible, older USB cables will also see a boost in speeds as great as 2 Gbps. USB 3.2 will also support USB-C connectors and their features such as power delivery, alternate modes, and digital audio, video and data on the same cable.

 

Overall, the new USB 3.2 standard is a big upgrade in terms of speed, but otherwise, it’s not a huge shift – which might be good news for those not ready to replace all of their older USB equipment. Though faster speeds are always good news, so this update is sure to be a welcomed change.

 

USB 3.1 Gen 1 vs. Gen 2

August 9, 2018 at 8:00 AM

 

Not sure of the difference between USB 3.1 Gen 1 (aka SuperSpeed USB) and USB 3.1. Gen 2 (aka SuperSpeed USB 10 Gbps or SuperSpeed+)? Don’t worry, you’re not alone. USB has rebranded and restructured how it differentiates between the two, leaving many scratching their heads as to which is which. Have no fear though, we’ve got it all figured out and are here to clear it up for you.

 

If you were impressed by the super speeds brought to you courtesy of USB 3.1, then you’re going to be over the moon for USB 3.1 Gen 2. This iteration of USB technology bolsters speeds and delivers additional benefits sure to please all users. As its name suggests, SuperSpeed+ USB increases the data transfer rate from 5 Gbps to 10 Gbps, making it twice as fast as USB 3.1 Gen 1 and on par with first generation Thunderbolt technology. USB 3.1 Gen 2 also uses more efficient data encoding, which not only increases throughput, but also improves I/O power efficiency.

 

Though the maximum cable length is shortened from 5 meters to 1 meter, USB 3.1 Gen 2 maintains the capability of data plus power over one cable and it can support multiple cameras and the USB3 Vision standard. Plus, USB 3.1 Gen 2 increases the power delivery level from 4.5 Watts to an astounding 100 Watts. This standard will also support USB Type-C, USB DisplayPort over Type-C and USB Power Delivery.

 

USB 3.1 Gen 2 is fully backward compatible with existing USB 3.0 software and devices, 5 Gbps hubs and devices as well as USB 2.0 products. In case there’s still some lingering confusion, here’s a handy chart to help compare these two side-by-side.

  

 

USB 3.1 Gen 1

USB 3.1 Gen 2

Data Rate

5 Gbps

10 Gbps

Power Delivery

4.5 W

100 W

Max Cable Length

5 m

1 m

Multiple Cameras

P

P

USB3 Vision

P

P

Data + Power

P

P

 

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845