Power of USB Power Delivery

February 21, 2019 at 8:00 AM

 

In this blog, we’ve talked a lot about USB. From USB 3.1 to USB 3.2, and even vibration-proof USB, USB is always reinventing itself, so it’s no wonder that it remains a powerfully popular interface. Now, USB is taking another step in its progression with USB power delivery, a fast charging technology with significantly higher power levels than standard charging. Here, we’ll take a look at the power of USB power delivery.

 

In the beginning, USB was merely a data interface that was able to provide a limited supply of power. Today, USB has evolved into a main power provider with a data interface. Thus, many things now use USB ports including cars, aircraft, laptops and wall sockets to charge or power devices and transfer data easily. In order to build on these existing USB functions, USB power delivery (USB-PD) has been developed to allow for maximum functionality of USB by delivering data and increased flexible power over a single cable.

 

USB-PD increases power levels from current standards and boosts them up to 100W. This allows for larger, USB-PD-enabled devices, such as tablets and laptops, to be charged over a USB-C cable without the use of bulky power cables. USB-C cables were designed to be able to handle the increased wattage of USB-PD without overheating or being damaged. USB-PD also enables the freedom of power direction that is not fixed, allowing the host or peripheral device to provide power. With USB-PD, enabled devices are capable of power management that is optimized across multiple peripherals, allowing each device to use only the power it needs. Additional power can be given as it is required for a specific application. This system also provides intelligent and flexible power management through hub communication with the PC. Plus, low-power devices, such as headsets, can negotiate to receive only the power they need. USB-PD specifications have been added to both USB 2.0 and 3.0 adopter agreements.

 

With the introduction of USB-PD, USB continues to prove itself an indispensable interface relevant in today’s continually changing world of technology.

 

USB 3.1 Gen 1 vs. Gen 2

August 9, 2018 at 8:00 AM

 

Not sure of the difference between USB 3.1 Gen 1 (aka SuperSpeed USB) and USB 3.1. Gen 2 (aka SuperSpeed USB 10 Gbps or SuperSpeed+)? Don’t worry, you’re not alone. USB has rebranded and restructured how it differentiates between the two, leaving many scratching their heads as to which is which. Have no fear though, we’ve got it all figured out and are here to clear it up for you.

 

If you were impressed by the super speeds brought to you courtesy of USB 3.1, then you’re going to be over the moon for USB 3.1 Gen 2. This iteration of USB technology bolsters speeds and delivers additional benefits sure to please all users. As its name suggests, SuperSpeed+ USB increases the data transfer rate from 5 Gbps to 10 Gbps, making it twice as fast as USB 3.1 Gen 1 and on par with first generation Thunderbolt technology. USB 3.1 Gen 2 also uses more efficient data encoding, which not only increases throughput, but also improves I/O power efficiency.

 

Though the maximum cable length is shortened from 5 meters to 1 meter, USB 3.1 Gen 2 maintains the capability of data plus power over one cable and it can support multiple cameras and the USB3 Vision standard. Plus, USB 3.1 Gen 2 increases the power delivery level from 4.5 Watts to an astounding 100 Watts. This standard will also support USB Type-C, USB DisplayPort over Type-C and USB Power Delivery.

 

USB 3.1 Gen 2 is fully backward compatible with existing USB 3.0 software and devices, 5 Gbps hubs and devices as well as USB 2.0 products. In case there’s still some lingering confusion, here’s a handy chart to help compare these two side-by-side.

  

 

USB 3.1 Gen 1

USB 3.1 Gen 2

Data Rate

5 Gbps

10 Gbps

Power Delivery

4.5 W

100 W

Max Cable Length

5 m

1 m

Multiple Cameras

P

P

USB3 Vision

P

P

Data + Power

P

P

 

 

Hot off the Presses - L-com’s 2018 Master Catalog

January 25, 2018 at 8:00 AM

 

The big reveal is here and we’re ready to share our 2018 Wired & Wireless Product Guide full of thousands of products including many new and best-selling items. Long regarded as a valuable resource for technicians, engineers and educators, L-com’s master catalog is packed with tips, tutorials, full-color product images and more, making it an excellent reference guide and educational tool.

 

Here are some of the new products featured this year:

·       M12 Ethernet Cabling for Harsh Environments

·       Continuous Flex Industrial Cables

·       HDMI High Flex Cables

·       Outdoor-Rated Ethernet Assemblies

·       Premium Panel Mounted Mini Coupler Kits

·       IP68-Rated Ruggedized LC Plugs and Receptacles

·       USB 3.1 Adapters

·       Category-Rated IP67 Bulkhead Shielded Panel Mount Couplers with Dust Cap

·       Heated 14x12x6 Enclosures

 

Getting a copy of our Wired & Wireless Product Guide is easy, simply fill out our online product guide request form and we will mail it to you straight away. You can also view this year’s catalog as a flip book or download pages from the product guide as PDFs.

 

Engineers’ Choice

October 13, 2016 at 8:00 AM

 

We depend on our engineers for their innovative ideas. We asked them what topic, technology or trend they thought we should feature in this weeks post. Our engineers’ choice: USB Type-C connectors. Here is an inside look at the connectors that got our enigneers’ stamp of approval.

 

We all love using USB. The plug-and-play interface makes it easy to connect and charge our devices. But it can be aggravating to figure out which USB cord goes with which device, and then which end plugs in where. Forutnately, our prayers have been answered and the technology gods have given us Type-C connectors.

 

USB Type-C is a tiny connector that boasts fast speeds, more power handling capabilities and a simpler, sleeker design.

 

The smaller, slimmer USB Type-C is a single connnector that can be used on all devices. Designed to replace both full-sized USB connectors as well as micro-USB connectors, it is tailored to fit mobile devices, yet powerful enough to be used with laptops and tablets. Whether you’re connecting an external peripheral to your laptop or charging your smartphone, Type-C connectors provide one cable small enough and powerful enough to do it all.

 

The Type-C connector has a simple, reversible design that makes using USB easier than ever. Completely reversible plug orientation and cable direction eliminate the guess work and frustration of not knowing which end is up when plugging in your USB devices.

 

Made for SUPERSPEED+ USB 3.1, Type-C connectors boast lightning speeds of up to 10 Gbps. They also support a vareity of different protocols that, with an adapter, allow output of HDMI, VGA, DisplayPort and other types of technologies from a single USB port. Type-C connectors are designed to provide scalable power and performance to adapt to whatever your future needs may be.

 

Type-C connectors are also made to support  USB Power Delivery (PD). Currently, a USB 2.0 connection provides up to 2.5 Watts of power, that’s enough to charge your phone, but not your laptop. With USB PD, the power delivery is increased to up to 100 Watts, and the power is bi-directional so it can be sent or received. That means that as long as the device and cable support USB PD, you can use a Type-C connector to charge devices from one another and possibly eliminate the need for a separate laptop charging cord.

 

Though USB technology is backward compatible, Type-C connectors are not, so we will continue to see devices and cords with both Type-A and Type-C connectors. Type-C connectors have been integrated into an increasing number of devices over the past year, they are now found on Google’s Chromebook Pixel and Apple’s MacBook and in the furture they may even replace Lightning connectors on iPads and iPhones.

 

For more information on Type-C connectors and USB 3.1, check out our blog post USB 3.1 – Fasten Your Seatbelts

 

USB 3.1 Gen 1 - Fasten your Seat Belts!

July 16, 2015 at 10:00 AM

 

It's a bird! It's a plane! No, it's SuperSpeed USB!

 

Your data transfer rates will soar to heroic speeds with the launch of USB 3.1 Gen 1, also known as SuperSpeed USB, which boasts three main advantages: speed, power delivery and the new Type-C connector.

 

As its name suggests, SuperSpeed USB delivers data transfer rate up to 5 Gbps, That makes it 10x faster than Hi-Speed USB and it provides power of up to 45 Watts. Plus, it minimizes user wait time because it is a Sync-N-Go technology.

 

SuperSpeed USB delivers optimized power efficiency with no device polling and lower active and idle power requirements. It is able to negotiate power, which allows two devices to decipher which one powers the other and the power direction can be changed without switching the physical cable direction. USB 3.1 Gen 1 is also backward compatible with previous versions of USB as far back as USB 2.0.

 

With USB 3.1 Gen 1 supporting USB Type-C, charging becomes easier than ever with the Type-C connector and its simple, reversible design that takes the guess work and frustration out of plugging in your USB devices. The smaller and slimmer Type-C connector will replace both full-sized USB connectors as well as micro-USB connectors, though there will be USB 3.1 Gen 1 cables that are backward compatible with existing USB 3.0 ports.

 

Set to launch in late 2015 or early 2016, USB 3.1 Gen 1 is coming to market as a single-cable solution supporting video, audio, data and power.  With this super-charged USB delivering more speed, more power and a sleeker, fool-proof design, USB is likely to remain the de-facto interface connecting your devices.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845