5 Things You Need to Know About the Cloud

August 31, 2017 at 8:00 AM

 

If you’re like most people, you probably have pictures or some other type of files stored in the cloud, but do you really understand what the cloud is? For many people, the cloud remains a mystical place that they still can’t quite comprehend. Here are 5 things you need to know about the cloud:

 

1.  When something is stored in the cloud, it is actually in a physical place. The cloud is like a giant IT data center, it is a massive infrastructure of thousands of servers that are connected by cables, switches, connectors and patch panels. All of these parts work together to store data, provide virtual desktops, global data access and more.

 

2.  Cloud computing relies on many geographically dispersed servers that provide millions of people with reliable and limitless access to their library of and images, video, audio and data files through the Internet. This frees up local RAM and hard drive space, but it also means that the interconnect components that make up the cloud need to be fast and dependable to keep up with user demand.

 

3.  The consumer cloud is different than a cloud for business. Consumer cloud computing is for those using cloud Internet services casually at home or in small offices. When it comes to business, there are several cloud models being used:

 

-  Software-as-a-Service (SaaS) – businesses subscribe to an application that is accessed using the Internet

-  Platform-as-a-Service (PaaS) – businesses create their own custom application for everyone in the company      to use

-  Infrastructure-as-a-Service (IaaS) – the big names in tech (Amazon, Google, Microsoft, etc.) provide a              backbone that can be used or “rented” for use by other companies

 

4.  The cloud is big business and is having a big impact on business. Worldwide public cloud services are anticipated to grow 18% this year to reach $246.8 billion. Cloud computing is also expected to be the most measurable factor impacting businesses in 2017. Cloud platforms allow for more complex business models and coordination of globally integrated networks – more so than many experts predicted. Cloud services are also increasingly being used by small and medium businesses, which is also increasing the revenue forecast.

 

5.  The Internet of Things (IoT) continues to grow, and with the IoT has come increased use of cloud computing technology. Eventually, IoT devices may become extensions of cloud data centers.  The cloud is a powerful force in the technology industry and a global trend that doesn’t seem to be slowing down.

 

Posted in: Wireless

Tags: , , , , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845