802.3bu - Power Over Data Lines (PoDL)

October 25, 2018 at 8:00 AM

 

In the realm of IEEE standards, 802.3 has some pretty good tricks up its sleeve. There is 802.3bt which expanded the capabilities of Power over Ethernet (PoE), 802.3bv brought you Power over Plastic Optical Fiber (POF) and 802.3bz which delivers 2.5 Gbps and 5 Gbps speeds data over copper. Now, the IEEE has unveiled 802.3bu – a standard for Power over Data Lines (PoDL).

 

Initially, single-pair Ethernet was created to help meet a demand in the automotive industry for Ethernet connectivity in vehicles. 802.3bu defines the specifications and standards for delivering power over single twisted-pair to connect Data Terminal Equipment (DTE) with IEEE 803.2 interfaces. This standard also extends the wattage range to up to 60 Watts of power, which is more power over a single cable than the PoE standards 802.3af and 803.2bt. With this PoDL standard, the most recent physical layers of single twisted-pair Ethernet are supported, including 100BASE-T1 and 1000BASE-T1, while using unshielded twisted-pair cables. This results in a lower cost and lighter weight solution, which is always good news. It is targeted for use in automotive, industrial automation, air and rail transportation, and other applications that use 100BASE-T1, 1000BASE-T1 or any single-pair data or non-data entity protocol. The IEEE 802.3bu standard also opens itself up for the possibility of additional applications across a variety of industries in need of solutions to adapt to the Internet of Things (IoT) expansion.

 

The goal of the 802.3bu standard is to specify a power distribution technique for use over a single twisted-pair cable that will allow for operation if data is not present. This standard is designed to deliver power that supports multiple voltages and classes of power at each voltage level. Plus, it has the capability of fault protection and detection to identify device signatures and communicate directly with devices to ensure precise and safe power delivery. PoDL supports fast startup operation with predetermined voltage configurations and the option of operation with run-time voltage configuration. It ensures compatibility with the IEEE 802.3bp standard. However, it is not compatible with Ethernet applications that operate over 2 or 4-pairs of twisted-pair cable.

 

With the introduction of 802.3bu PoDL, not only is the wattage delivery increased and intuitive, the possibilities of power delivery are increased as well.

 

802.3bv - The Power of Plastic Optical Fiber

August 16, 2018 at 8:00 AM

 

In the realm of IEEE standards, 802.3 is bringing a lot to the table for today’s newest innovations. This standard includes several iterations that support ground breaking technology, including 802.3at and 802.3bt that support Power over Ethernet (PoE), 802.3bz that delivers 2.5 and 5 Gbps speeds over copper and now we can add 802.3bv to that list. 802.3bv was developed to support Power over Plastic Optical Fiber (POF) and it’s slated to deliver groundbreaking speed and performance.

 

First, let’s take a look at plastic optical fiber and all of its capabilities. It is a large core, step-index optical fiber capable of speeds of up to 1 Gbps. It is easy to install, cost effective, durable and is an ideal choice for networks reaching 80 meters with infrastructure that connects to switches and/or wall plates. POF will be able to meet the higher bandwidth demands of developing technology and can be used in new applications for home, industrial and automotive networks. Thus, there has been a push for the development of 802.3bv to support all of the possible POF applications.

 

The IEEE 802.3bv standard is an amendment to the 802.3 standard that allows 1000 Mb/s speeds, allowing POF to meet the increased bandwidth needs of those automotive, industrial and home network connectivity applications. 802.3bv delivers Gigabit Ethernet operation over POF and defines physical layer specs for home, industrial and auto industries. With 802.3bv, POF Ethernet networks will have the support of a robust and reliable media option. Automotive applications will have operation over a minimum of 15 meters with 4 POF connections, and distances of at least 40 meters with zero POF connections. Home and industrial applications will be able to achieve lengths of at least 50 meters with one POF connection.

 

There are three physical layer specifications in this amendment, specifically designed for the industries targeted. All use 1000BASE-H encoding over duplex POF cable and red light wavelength transmission.

 

  • ·        1000BASE-RHA – 1000 Mb/s speeds for home network and consumer applications 

 

  • ·        1000BASE-RHB – 1000 Mb/s made for industrial applications

 

  • ·        1000BASE-RHC – 1000 Mb/s rates designed for automotive applications

 

With the development of 802.3bv, yet another layer of power and possibility has been added to the realm of IEEE standards, ensuring that the world of technology has no intention of slowing down.

 

Plastic Optical Fiber (POF) Pros and Cons

April 26, 2018 at 8:00 AM

 

In our previous blog posts, we’ve explored many of the advantages of fiber optic cables. From faster speeds, greater bandwidth, immunity to EMI/RFI and better performance in harsh environments, fiber has a lot of advantages over traditional copper cabling. We’ve also compared multimode fiber vs. single-mode fiber. But what about plastic optical fiber (POF)? Here, we’ll explore the good and the bad of POF and how it can work for you.

 

Plastic Optical Fiber is a large core, step-index optical fiber that can deliver data rates of up to 1 Gbps. POF is an ideal choice for networks with infrastructure runs of up to 80 meters connecting to switches and/or wall plates. Because it’s made of plastic, POF is more durable and is easily installed in minutes with fewer tools and less training.  It is also priced more competitively, which makes it a more attractive option for desktop LAN connections and low-speed short links.

 

POF will support the higher bandwidth demands projected for the average user in the coming years. It is also well-suited for developing new applications that require higher bandwidth, including IPTV and Triple Play services. It can be used in businesses, homes, student housing, apartments and condos. As a matter of fact, the IEEE recently specified the 802.3bv standard for plastic optical fiber. This standard will allow POF to provide Gigabit Ethernet support for applications such as automotive, industrial and home networks.

 

With a typical diameter of 1 mm, POF is about 100 times larger than glass optical fiber, which could be a downfall, but the large size allows it to easily couple a large amount of light from sources and connectors that don’t have to have high precision. This makes termination simple and cuts connector costs by an average of 10-20% compared to glass fibers.

 

POF is ideal for short-range communication networks and plays an important role in military communication networks. It is also safer than glass optical fiber because it uses a harmless green or red light that is easy visible to the eye. Though plastic optical fibers can’t withstand the extreme high-temperatures that glass optical fiber can, they do provide added durability and flexibility for use in data communications, industrial environments and military applications.

 

The list of cons is short: slower data-rates, shorter distances.  

 

POF has a lengthy list of pros. Here’s an overview:

 

·       Lower cost

·       Easier to install

·       Less infrastructure support required

·       50% less power than copper

·       80% less carbon dioxide than copper

·       High-performance data transfer

·       Resists EMI/RFI and crosstalk interference

·       Lightweight and durable

·       Waterproof, moisture-proof and magnetic-free

·       LEED-certified

·       Future 802.3bv standard (1Gbps speeds)

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845