DJ Drops Mad Beats But Not His USB Connection

March 6, 2014 at 10:00 AM

A Testimonial from the Nerdy DJ (DJ Forge)

 

 

A USB dropout.

 

The mixer isn’t communicating with the software and silence starts to creep in as people halt to a standstill on the dance floor. Alternative sound must recover or else dead air lingers until the equipment is either trouble-shot or rebooted.

 

This is a DJ’s worst nightmare. Everything counts when you’re mixing in a club or at a large show. A lag or halt in the music is a death knell.

 

That’s why Jordan Chavis, better known as DJ Forge of North Carolina, must rely on fail proof equipment (including high performance cables) to run his shows. According to Chavis, anything you can do to avoid that dropout scenario is a win. Having the right USB cable is just a small but important part of his set-up.

 

So, Chavis turned to L-com’s Right Angled USB Cable to run his DJ mixer. “You can tell the difference between a high quality cable and cheap cable,” Chavis said, “And this one has been really reliable.”

 

Chavis discovered L-com’s Right Angled USB Cable when he was faced with an unusual USB port placement on a trial piece of equipment. On his blog called The Nerdy DJ (for working DJs, by working DJs) Chavis and his friends did a comparison of two mixers and wrote about it in Rane Sixty-Two vs. Pioneer DJM-900SRT. Since the USB port was on top of the Pioneer DJM-900SRT mixer instead of in the back where it normally is, he decided that he needed a cable which would be secure yet flexible.

 

Armed with his Right Angled USB cable, Chavis is confident he can run his shows without skipping a beat.

 

“This cable is something that my DJ friends and colleagues and I will recommend to use for all types of DJ mixers or DJ controllers,” said Chavis, “Because even if the port is in the back, it’s convenient to have the right angle for connection security and it get’s the cable out of the way.”

 

In addition to providing equipment reviews like the Rane vs. Pioneer demo, Chavis’s website is a community for DJs to turn to for career advice, how-to’s, maintenance tips, and more. Chavis aspires for Nerdy DJ to be a place where DJs are collaborating and a site that every DJ wants to check when he or she wakes up in the morning. Alongside playing weekly shows and serving as the official UNC DJ, Chavis has focused his time working hard on Nerdy DJ since last October so that it can be a hot spot for new and old DJs alike.

 

Chavis has opened for some of the biggest names in hip-hop including Jay-Z, Young Jeezy, Fabulous, Clipse, KRS-One, Ghostface, Method Man, and more. He discovered his love for DJing back in college as a computer science major, when a roommate brought back a turn table to their place.

 

“I got nerdy about DJing instead of nerdy about coding,” said Chavis.

 

In the upcoming weeks you can find DJ Forge at events in some of his favorite spots in NC. Chavis said he is also starting to throw hip-hop shows once a month and hopes to narrow his focus on growing in his career, as well as travelling more. Keep a lookout for him in Tokyo or elsewhere in Japan in the near future!

 

Photo by Jordan Chavis

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845