Industrial Enclosures for any Application

October 4, 2018 at 8:00 AM

 

When it comes to protecting your valuable equipment, a NEMA enclosure can be a great solution. Whether your equipment could be exposed to the elements, chemicals, human tampering or theft, using an enclosure can ensure your investment is protected and provide you with peace of mind. Different enclosures provide different benefits, and you must find the best fit for your application. Here, we’ll take a closer look at Industrial enclosures and all that they have to offer.

 

When it comes to location, industrial enclosures can be used for both indoor and outdoor applications. In any setting, industrial enclosures provide extra security against theft, tampering and damage. Standard enclosures are lockable and keyed locks can be added as an extra measure to keep valuable components safe. Weatherproof outdoor enclosures can provide superior protection from the elements for outdoor wireless access points and sensitive electric components. Plus, with the option of adding heating and cooling or power, these enclosures deliver dependable performance in any climate.

 

There are numerous features that make industrial enclosures ideal for protecting sensitive equipment, these include mounting plates that securely mount equipment inside an enclosure and a thermostat controlled cooling fan that keeps equipment cool in high temperature environments. Also, a mounting lid can prevent damage and theft of the equipment inside the enclosure, these lids can have hinges, removable lids or clear viewing windows for easier viewing while maintaining security. Power over Ethernet (PoE) interface is another great feature that delivers power to the enclosed equipment where power sources are limited, plus it provides additional surge protection for internal PoE compatible equipment.

 

Many applications can benefit from the use of an industrial enclosure, and while the details might vary, they all share a similar set of requirements that include being able to operate under exceedingly harsh conditions that include exposure to corrosive chemicals, extreme temperatures and more. Some of these applications include industrial automation, oil and gas, and transportation. Rugged, industrial enclosures are also ideal for security and automation applications such as access controls, fire alarms, video surveillance equipment and building automation.  Indoor and outdoor enclosures can be used in a variety of locations to protect equipment, including cell towers and rooftops, open-access basements, telecom closets, shopping centers and factories.

 

Overall, industrial enclosures are a great way to keep expensive equipment safe. In almost any application, and even in the harshest conditions, they provide a level of security that is unmatched. To take a look at L-com’s complete, comprehensive line of industrial enclosures, click here.

 

Case Study: Lineage Logistics

May 10, 2018 at 8:00 AM

 

As the second largest cold storage thrid-party provider in the US, Lineage Logistics provides cold storage solutions for leading grocery, food and retail  companies.

 

During a wireless network roll-out in their warehouses, Lineage Logistics needed to add multiple access points inside refrigeration units with temperatures as low as -40 degrees. The company’s engineers had designed a wireless access point that fulfilled the needs of the project, but wasn’t able to function unprotected in the cold temperatures.

 

Lineage Logistics began searching for an enclosure that would protect their access point, offer Power over Ethernet (PoE) over a single cable and meet cost requirements.

 

After rejecting a competitor’s offering, as it didn’t fully meet the requirements, Lineage Logistics came to L-com for help. Our team was able to develop a comprehensive solution that met all their needs. We created a custom NEMA enclosure that could house the access point and provide plently of room if adjustments were needed. We were also able to save Lineage Logistics time and money on installation by mounting the access points in the enclosures and providing all required cabling and antennas.

  

L-com was able to not only meet, but surpass this client’s expectations with the perfect solution to their problem.

 

To read the full case study, click here.

 

White Paper: Wireless Antenna Mounting

March 15, 2018 at 8:00 AM

 

The key to any wireless network is the wireless antenna. It is the hub to which all other parts rely. When determining the right antenna for your application, you must first consider the best location for your antenna, then you have to figure out how to mount that antenna. Our white paper takes an in-depth look at different antenna mounting options for directional and Omni-directional antennas.  

 

Here are some of the common installation options covered for antennas and access points:

 

NEMA Enclosure Mounting:

  •       -   Typical configurations run a pigtail cable from the access point or radio to a bulkhead N-female adapter or coax lightning protector, then attach the antenna directly to the adapter or lightning protector
  •       -   Antennas can also be mounted remotely

 

Pole Mounting:

      -  Using rugged, clamp-style mounting brackets included with most of L-com’s Omni-directional antennas

      -  Upper and lower articulated clamp mounts used with sector-style antennas

      -  Yagi and patch-style antennas use tilt and swivel clamp mounting systems

 

Side of Building Mounting:

      -  HGX-UMOUNT can be used to mount antennas to the side, roof parapet or under the roof eaves of a building.

 

Mobile Mounting:

      -  Several options are available for mobile mounting, including magnetic mounts, NMO bulkhead-style mounts and using a CA-AM1RSPA010 mobile mounting cable

 

Window Mounting:

      -  Suction cups can be used for window mounting

 

Outdoor Access Point Mounting:

      -  Pole mounting or wall mounting are typically utilized for access points

      -  A NEMA enclosure might be needed to protect the access point, surge protectors etc.

 

Click here to read our Wireless Antenna and Access Point Mounting white paper.

 

All our free white papers are available from our website by clicking here.

 

NEMA Enclosures: Best Fit Guide

July 7, 2016 at 8:00 AM

 

With so much relying on your network being fully functional, a NEMA enclosure is one of the best ways to safe-guard your valuable equipment. NEMA enclosures are ideal for wired and wireless networks to protect critical equipment from the elements, chemicals, physical contact, theft and damage. They are designed to endure all types of abuse and keep enclosed, sensitive electronics safe.

 

The National Electrical Manufacturers Association (NEMA) rates enclosures based on criteria that includes resistance to dust, moisture, water immersion and ice. The better the rating, the more the enclosure can withstand.

 

Here, we guide you through the most popular enclosure features to help find the best fit to protect your valuable equipment.


Industrial

Most enclosures are labeled as “industrial” because they are built to be rugged and protect against the elements and feature options such as heating and cooling. They are made for indoor and outdoor use in hot and cold environments.


Weatherproof

When your equipment is located outside or in an industrial setting, such as a factory or processing plant, a weatherproof NEMA enclosure provides the insurance you need. They protect against damage from environmental hazards such as water, dust, oil and corrosive chemicals like gasoline.


Non- Powered

These protective enclosures are perfect for wired and wireless communications equipment that do not require power. L-com’s non-powered enclosures feature fully gasketed lids to ensure optimal performance. Our non-powered enclosures are also available in a variety of rugged materials including Molded Fiberglass Reinforced Polyester (FRP) and VALOX 357U thermoplastic material.

 

Powered

For equipment that requires a power source, a powered NEMA enclosure will be your best bet. They share many of the same attributes as their non-powered counterparts but can be built with power outlets for various interfaces including 12V DC, 120V AC, 240V AC and POE. Some powered enclosures also include built-in lightning protection for an extra level of security.

 

Heating and Cooling

If your equipment will be exposed to cold temperatures, extreme heat or moisture, you may want a NEMA enclosure that provides cooling, heat or ventilation. For example, L-com offers an enclosure that is ideal for keeping equipment warm and functional in sub-zero temperatures as low as -30°F (-34°C). This particular model features a thermostat-controlled heating system that is powered by a Cat5 cable and is shielded by foam insulation and fiberglass.

 

NEMA enclosures provide plenty of options that can be mixed and matched to make sure your network equipment is protected. For more information on which options will be the best fit, or to have us design a custom enclosure for you, contact us today.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845