Embedded Antennas and the IoT

May 2, 2019 at 8:00 AM

 

In the not so distant future, the world will be fully automated with machines being able to communicate with little or no interaction from humans, thanks to the arrival of the Internet of Things (IoT) and the use of embedded antennas.

 

These small form factor antennas are a perfect fit for the shrinking size of IoT devices, while still being able to keep up with the massive amounts of data that will need to be transmitted as the IoT connects physical devices with software based management and control applications.

 

Embedded antennas are small, yet powerful antennas with many offering multiband support for use in mobile and fixed data applications. Their key performance attributes include high efficiency, low power consumption, low return loss and isolation.

 

High efficiency brings better signal reception, improving the system’s ability for faster data transfer rates. Reduced power consumption allows for increased longevity. Less return loss means more power transmitted, and isolation limits the amount of crosstalk interference. Embedded antennas can work with high-frequency or low-frequency systems, some feature MIMO technology and smart antennas have been introduced that feature embedded GPS and Flash memory capabilities.

 

As IoT deployments get underway, there are more embedded antenna options to consider to take full advantage of this exciting era of automation.

 

To help you succeed with your IoT implementations, we offer a full line off-the-shelf, embedded antennas ready to ship the same-day, plus custom designed antennas to suite all of your IoT needs.

 

5 Things You Need to Know About Industrial IoT

July 6, 2017 at 8:00 AM

 

With the Internet of Things promising a world that is fully automated where objects can communicate without humans, it only makes sense that this technology could be used in other ways –enter the Industrial IoT (IIoT). This next iteration of the IoT applies the IoT technology to industrial applications and is slated to revolutionize the way we do business. Here are 5 things you need to know about the Industrial IoT:

 

1.       It’s smart business

We’ve heard of smart houses, smart cars and even smart cities, now we’ll have smart businesses. The goal of the IIoT is to improve efficiency, productivity and operations on a global scale by linking people, data and intelligent machines. Machines will be able to communicate and work with each other in machine to machine (M2M) networks to optimize production and workflow. 


2.       It takes business into the Cloud

The IIoT integrates physical machinery with software and sensors that can be networked to the Cloud to provide real-time visibility of business assets. These smart machines deliver data that is analyzed and used to monitor and control operations and make real-time decisions, which improves operational efficiency, saves money and reduces waste.

 

3.       It is applicable across a range of industries

Pilot projects have tested and proven that the IIoT can be impactful across a large spectrum of industries that include healthcare, manufacturing, logistics, energy and agriculture.

 

4.       It breathes new life into old equipment

The IIoT will connect more than a century’s worth of existing mechanical and electrical infrastructure to the Internet. This includes manufacturing equipment, fleet tracking and HVAC systems. The IIoT has the power to reduce waste and improve operating costs with features such as a service alert sent before equipment breaks down, or monitoring the flow of gas valves in a refinery.

 

5.       It is the future of business

The IIoT is projected to be one of the fastest growing markets over the next several years with as many as 25 billion IP-enabled "things" being networked by 2020. It has been forecasted that the IIoT will generate nearly $320 billion in worldwide revenue and over 26% CAGR by 2020.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845