Embedded Antennas and the IoT

May 2, 2019 at 8:00 AM

 

In the not so distant future, the world will be fully automated with machines being able to communicate with little or no interaction from humans, thanks to the arrival of the Internet of Things (IoT) and the use of embedded antennas.

 

These small form factor antennas are a perfect fit for the shrinking size of IoT devices, while still being able to keep up with the massive amounts of data that will need to be transmitted as the IoT connects physical devices with software based management and control applications.

 

Embedded antennas are small, yet powerful antennas with many offering multiband support for use in mobile and fixed data applications. Their key performance attributes include high efficiency, low power consumption, low return loss and isolation.

 

High efficiency brings better signal reception, improving the system’s ability for faster data transfer rates. Reduced power consumption allows for increased longevity. Less return loss means more power transmitted, and isolation limits the amount of crosstalk interference. Embedded antennas can work with high-frequency or low-frequency systems, some feature MIMO technology and smart antennas have been introduced that feature embedded GPS and Flash memory capabilities.

 

As IoT deployments get underway, there are more embedded antenna options to consider to take full advantage of this exciting era of automation.

 

To help you succeed with your IoT implementations, we offer a full line off-the-shelf, embedded antennas ready to ship the same-day, plus custom designed antennas to suite all of your IoT needs.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845