Let us give you a general reminder that says a lot in just a few words:
Not all cables are created equal.
Have you ever considered that your application or next networking project might require more than a standard cable, whether it be USB, Ethernet, HDMI or other interface?
Of course, in either scenario you want a cable that is built to last. That’s why armored cables are built to stand up to the harshest of environments.
Armored cables are commonly used in factory automation, manufacturing networks, chemical and petroleum processing networks, and in any Industrial communication or Industrial HMI and A/V application.
For example, complex chemical and oil refining facilities employ some of the most sophisticated process control systems found in any industry. Mass-scale process control delivers consistently high system output (both quantity and quality) while simultaneously minimizing labor input and safety issues.
These results can only be achieved through the deployment of complex network control systems (including ruggedized cabling) that must operate under harsh conditions. Multiple control and monitoring points must interconnect in environments that include corrosive liquids and gases, severe heat and cold, high pressure and more.
If you take a closer look at the details of your environment, you might be surprised to find that at least one of these factors puts it into the “harsh environment” category.
L-com offers an extensive line of metal and plastic armored cable assemblies to address all types of these industrial and harsh environment connectivity applications.
Here are some common features you’ll find throughout our ruggedized cable selection:
- Choose from either metal armor that provides 1,500 pounds per square inch crush resistance to protect cables from damage, OR plastic tubing - that provides 800 PSI crush resistance.
- Heavy duty metal and plastic coupling nuts ensure armored sleeves remain anchored
- Cable shielding provides maximum protection against EMI/RFI
- Specially jacketed cable for use in hot/cold/corrosive environments (some types)
And for a detailed layout of the “behind the scenes” of how these cables are constructed, below are some diagram tutorials. Have a look and give us a call if you have any questions!
Armored D-Subminiature Cable Assemblies

Armored USB Cable Assemblies

Armored HDMI Cable Assemblies

Armored DVI Cable Assemblies

And last but not least: Armored Ethernet Assemblies.


All of L-com’s armored cable assemblies are available off the shelf for same day shipping with no minimum order quantities.