How Tech is Changing Transportation

April 19, 2018 at 8:00 AM

 

These days, it’s hard to find a part of our everyday lives that’s not being transformed in some way by technology. Transportation is no different. Driverless cars have been at the forefront of most transportation technology discussions lately, but do you know other ways that tech is changing how we get from point A to point B? Here, we’ll take a look at some of the ways technology is changing the transportation industry.

 

Rail

 

Railways are one of the oldest forms of transportation still used today. At their inception, trains were a groundbreaking way for people to get back and forth for everyday commutes, to explore places they’d never been and to transport goods at speeds that were unheard of at the time. Rail systems are still used today for many of the same reasons, but they are much smarter. Today’s rail yards have wired and wireless technology that allows for communication throughout the rail yard to provide security, control and real-time data collection.

 

RFID technology has also been put in place to modernize asset management in rail yard operations. Instead of employees walking from one car to another, manually recording inventory, today’s systems use electronic scanners to record asset information accurately and without the variable of human error. This data is then sent back to a central office where assets can be monitored in real time.

 

Technology is also being used to make rail travel safer by using wayside monitoring applications to record real-time data such as speed, time of passing and track conditions. This critical information is used for real-time scheduling and to generate safety alerts.

 

Roadways

 

Until all of those self-driving cars get on the road, and possibly still after, making roadways safer is another way technology is affecting the transportation industry. In tunnels, cellular and Wi-Fi service are provided by antennas while IP cameras connect to an Ethernet network. These cameras provide real time surveillance to a tunnel control center, so traffic and safety concerns can be monitored live. Digital signs are also connected to the Ethernet network, allowing them to be controlled remotely.

 

Intelligent Transportation Systems (ITS) use wired and wireless technology to control roadway traffic signals and vehicle and pedestrian safety systems. These systems utilize technology to manage traffic flow and ease congestion on the roads. Roadway security and overall safety is also improved with IP cameras and traffic sensors providing live surveillance and control.

 

With the use of wireless technology, roadside digital signs are able to deliver real time messaging along roadways with live updates being delivered from a central control office. These messages can include weather updates, traffic and road condition alerts and information on alternate routes, all of which can make travel easier, more efficient and save lives.

 

Maritime

 

An entire ship, including every part of shipboard communications and surveillance, can be managed via a central management station by using an Ethernet network and Simple Network Management Protocol (SNMP). 

 

IP cameras are used for monitoring, cables connect propulsion and steering systems to a controller, and antennas allow for voice and data communications and RFID management of cargo containers.

 

To load and unload ships, modern seaport terminals use automated crane systems to save freight companies millions of dollars in labor, maintenance and repairs. Computers are housed in a secure location, connected to Ethernet networks and used to control the cranes. This wireless network allows remote control over operations without the cost of running cables.

 

On the dock, keeping track of personnel, assets and ground support vehicles is made easier with wireless communications. Antennas allow for communication with the central operations command center. They also support Intermodal container RFID tracking systems which enable wireless devices to quickly and accurately process container and inventory information in real-time. With cellular and Wi-Fi communication between crews, freight companies can save money and increase security by eliminating the need for traditional radio communications.

 

For an in-depth look at what L-com products are being used to deliver technology to the transportation industry, click here.

 

Read All About It: PoE White Paper

August 3, 2017 at 8:00 AM

 

Power over Ethernet (PoE) is a revolutionary technique that provides both power and data in one Ethernet cable. PoE equipment eliminates the need to run power to remote network devices, which allows for greater flexibility and is ideal for remote locations where traditional power sources are not available. PoE can save time and money and is becoming more frequently used in wired and wireless connectivity applications with network devices such as wireless access points, switches and IP cameras.

 

Our white paper takes a deeper look at PoE, its history and how it is used in today’s telecommunications networks. Topics covered include:

 

History of PoE

  • -          How the IEEE was called upon to create the 802.3af standard to help the growth of the PoE market with a unified standard              to rely on
  • -          Power Sourcing Equipment (PSE)
  • -          Powered Devices (PD)

 

PoE Details and Variations

  • -          Mode A vs. Mode B
  • -          Mode A: Combining power via Phantom Powering
  • -          Mode B: Power over Ethernet spare pairs

 

Click here to read our PoE white paper.

 

All of our free white papers are available from our website by clicking here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845