Readers’ Choice -Top Blog Posts of 2018

December 20, 2018 at 8:00 AM

 

Our goal for this blog is to provide interesting and informative content for our readers. So we always enjoy taking a look back at the end of the year to see what the most popular posts were. To make sure you didn’t miss anything, here’s a list of the most read posts of 2018. We hope to see you back in 2019!

 

 

1.      Cat6 Cable: Shielded vs. Unshielded


Category 6 Ethernet cable is designed to provide high speed data rates, but how do you decide between shielded or unshielded? Here, we compare them side by side so you can choose which will work best for your application. Read more.

 

 

2.      10 of the Worst Cabling Nightmares

 

We pride ourselves on our commitment to provide the best connectivity solutions for our customers, helping them to manage their data centers. So it always comes as a shock when we see cabling infrastructure that is a complete nightmare. This post has some of the worst offenders we’ve seen on the web. Read more.

 

 

3.      The Advantages and Disadvantages of Shielded Ethernet Cable

 

When it comes to shielded Ethernet cable, there are pros and cons. This post takes a look at both the good and the bad to help you weigh your options. For example, shielding can offer protection from EMI/RFI but its weight and limited flexibility means it’s not ideal for every application. To help decide if shielded Ethernet cable is right for your installation, read the post.

 

 

4.      75 Ohm vs. 50 Ohm – Coaxial Comparison

 

Ohm may sound like something you’d say while meditating, but when it comes to coaxial cables, it is actually a unit of resistance. Ohms measure the impedance within the cable. Impedance is resistance to the flow of electrical current through a circuit. To see how 75 Ohm and 50 Ohm compare, read our post.

 

 

5.      Good Vibrations: Vibration-Proof USB Connectors


Universal Serial Bus (USB) is one of the most widely used technologies to connect and power devices. One fundamental flaw of USB is its sensitivity to vibration, causing the connector to dislodge. In this post we show you some solutions to keeping your USB connected. Read more.

 

Readers’ Choice -Top Blog Posts of 2017

December 21, 2017 at 8:00 AM

 

As we wrap up another year, we’d like to take a moment to look back on some of our most popular posts. We pride ourselves on providing informative content for our readers by covering a range of wired and wireless technology topics. We sincerely hope that you enjoyed reading our posts as much as we enjoyed writing them and in case you missed anything, here’s a highlight reel of the most popular posts of 2017.

 

 1.       Cable Showdown: Cat6 vs. Cat6a

 

It’s a Cat eat Cat world out there and Cat6 and Cat6a are two of the most popular standards for Ethernet cables. So, how do you decide between the two? One may work better than the other, depending on your application. To help you pick a winner, we compared them side-by-side for a showdown of category proportions. To see how each Cat fared, read the post.

 

 

2.       White-Space Wi-Fi 802.11af

 

Waste not, want not, seems to be a growing way of life for many people these days, and that theme will soon apply to the Wi-Fi spectrum as well. The IEEE standard 802.11af, also known as white-space Wi-Fi or White-Fi, will utilize the unused space in the TV spectrum, the TV white-space, to support Wi-Fi networks. Read the post to find out how it all works.

 

 

3.       OM5 – The Next Generation of Multimode Fiber

 

OM5 was chosen to be the new standard for cabling containing wideband multimode fiber in the 3rd edition of the ISO/IEC 11801 standard. The acceptance of this standard is a milestone for the fiber cabling performance category because it extends the benefits of this revolutionary multimode fiber within connected buildings and data centers worldwide. To find what you need to know about OM5, click here.

 

 

4.       802.11ax – The Next Big Thing

 

The IEEE will be adding to its 802.11 series of standards again with the launch of 802.11ax. 802.11ax is under development and will pick-up where 802.11ac left off by taking MIMO to the next level with MIMO-OFDM. This next big upgrade to Wi-Fi networks might not make its debut for a couple of years, but here’s a look at what’s coming.

 

 

5.       75 Ohm vs. 50 Ohm – Coaxial Comparison

 

Ohm may sound like something you’d say while meditating, but when it comes to coaxial cables, it is actually a unit of resistance. Ohms measure the impedance within the cable. Impedance is resistance to the flow of electrical current through a circuit. To see how 75 Ohm and 50 Ohm compare, read our post.

 

 

Specialized Cabling Systems for Military Applications

April 6, 2017 at 8:00 AM

 

When you hear the word “military” you probably think of tanks, weapons and camouflage. Military communications and cabling systems may not be the first things that come to mind, but they certainly are an important part of military operations.

 

Cables being used in combat zones face more rigorous requirements than those used in everyday civilian applications. Military voice, video and data systems are designed for rapid deployment in harsh environments with exposure to extreme temperatures, shock, vibration, dust and moisture. Cables in these systems are also exposed to heavy EMI and RFI from motors, switching power supplies and nearby microprocessors, all of which can be detrimental to network performance.

 

These extreme conditions would render a commercial communications system useless, so combat-specialized infrastructure products have been designed to meet the needs of today’s combat-ready network systems.

 

Here are some examples of products and technologies designed to meet the needs of military communications networks.

 

Fiber Optics

 

By design fiber cables are immune to EMI and RFI sometimes encountered in the combat theatre. Additionally, fiber optic cables are now offered in special crush and impact-resistant designs and some military-styles are available with armored jacketed cable.

 

Connectors such as the Straight Tip (ST) are fitted with heavy tension springs to ensure proper mating when exposed to major shock and vibration. They are also offered with locking mechanisms for additional protection against optical disconnects.

 

Other fiber optic connectors for military applications feature Ingress Protection (IP) rated designs with screw lock mating and extra-strength strain reliefs of over 250 Newton’s to ensure a solid connection during field use.

 

Shielded Ethernet Cable

 

Shielded Cat5e or Cat6 copper cables are the way to go when fiber cabling isn’t an option. Military applications require shielded twisted pair (STP) copper cables and rugged military-style connectors for most applications. STP cabling reduces the damaging effects of EMI and RFI sometime encountered in the field.

 

Other Ethernet cabling options for military apps include IP68 rated cables that utilize ruggedized Anodized or Zinc Alloy finished connectors and double shielded, high-flex, UV and Oil resistant FR-TPE (Flame Retardant Thermoplastic Elastomer) jacket that is CMX outdoor rated to stand up to the toughest environments.

 

Jacket Compounds

 

Whether you’re using fiber or copper cables, the cable jacket compound should always be taken into consideration. The outer cable jacket of many copper and fiber cables is usually made of PVC material that is toxic when burned and can accelerate a fire spreading.

 

Low-smoke zero-halogen (LSZH) jackets are a much safer solution and a popular choice for military applications. As the name implies, LSZH cables produce minimal smoke and no halogen, both of which can be harmful to people and expensive communications equipment. LSZH cables will also self-extinguish which makes them ideal for enclosed spaces such as ships, aircraft, tanks and other vehicles.

 

Polyurethane jackets are sometimes used in military applications because of their ability to withstand damaging UV rays, oil and petroleum-based products, and mechanical abuse. Though cables with a Polyurethane jacket will also release toxic gases and will not self-extinguish like LSZH cables.

 

Cable Showdown: Cat6 vs. Cat6a

March 23, 2017 at 8:00 AM

 

 

Cat6 and Cat6a may be two of the most popular standards for Ethernet cables, but how do you decide between them?  Depending on your application, one may work better than the other. To help you decide, we thought we’d stack them up side-by-side for a showdown.

 

  

 

Both Cat6 and Cat6a offer speed, flexibility and cost savings. They can both be used for PoE applications and are ideal for transmitting voice, video and data, though Cat6a is able to move larger volumes of data. Cat6 cables are great for connecting access points and other devices including media converters, switches and wireless controllers that are typically running at 1Gbps speeds. Cat6a cables are typically used in data centers and storage area networks (SAN) that require 10Gbps connectivity or more through trunked 10Gbps connections.

 

The cost difference between the two is minimal. The main difference is that Cat6a is able to transmit at 10 Gbps supporting 10GBASE-T over longer distances than Cat6 cables. Cat6a also builds upon Cat6’s capability to protect against alien crosstalk, which improves performance. Though if a shielded cable isn’t necessary and a lighter option would work best, unshielded Cat6 has the advantage. As always, the requirements of your application will dictate which cable to use.

 

All Contacts are Not Created Equal

March 9, 2017 at 8:00 AM

 

Certain contacts work best on certain types of cable. Here, we’ll take a look at how to determine which type of contact is best for your application.

 

First, you need to determine which type of cable you’re using – solid or stranded. All cables will fall into these two categories no matter if they’re Cat5e, Cat 6 or otherwise. 

 

A solid cable’s conductors are made of solid metal, usually copper, making the cable more rigid.  Solid cables are typically used as infrastructure cabling in walls, ceilings and conduit where flexibility isn’t necessary since the cable is put into place and left alone. They are also cheaper, transmit better over long distances (lower attenuation than stranded cable), but they are more likely to break if bent repeatedly.

 

Stranded cables are much more flexible because the conductors are made of thin metal wires that are twisted together to create a larger, thicker conductor. These cables are frequently used as patch cords and shorter network cable runs that need extra flexibility for bending.  Stranded cables are typically more expensive than solid cables, but they work well for shorter distances and can stand-up to repetitive bending without breaking.

 

Now that you’re clear on solid versus stranded cables, we can take a look at the types of contacts that are available for RJ45 plugs that are used on Ethernet cables.

 

Each contact is designed for a specific cable type and not all plugs will work on all cables. 

 

The diagram below outlines that main contact designs that are available. Some contacts can be used on both solid and stranded cable. Always check the manufacturer’s datasheet to determine if the plug/contact can be used with your cable type.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845