All about Antenna Polarity

March 16, 2017 at 8:00 AM

 

Whether you’re installing one antenna or an entire tower-full of them, antenna polarization is one of the most important pieces of the puzzle to consider, yet it is also one of the least understood properties of wireless communication.

 

Most antennas are typically mounted horizontally or vertically and the way they are mounted determines their polarization. For the best network performance, antennas used in point-to-point wireless applications should have the same polarization as each other. A wireless links can be established with antennas of different polarity, but usually it compromises the network performance and connectivity.

 

Though there are some cases where using antennas with different polarization is beneficial in reducing interference. For example, if you’re mounting several antennas on a tower, your best plan is to stagger vertically and horizontally polarized antennas to decrease interference.

 

Some wireless applications won’t work with horizontal or vertical polarization. In these cases, there are other polarization schemes to explore including: dual-polarized, cross-polarized and circular-polarized antennas.

 

The diagram below outlines the different antenna polarity types.

Antenna Polarization: What’s It All About?

December 10, 2015 at 8:00 AM

 

If you’re not sure which side is up when it comes to antenna polarization, you are not alone. Antenna polarization may be one of the least understood properties of a wireless signal.  If you are installing many antennas in one location, like on a tower, polarization is an important piece of the puzzle that you’ll need to take into consideration. Here we give you a quick overview on antenna polarization.

 

Polarization is determined by the way an antenna is mounted, usually horizontally or vertically. To ensure optimal network performance only like-polarized antennas should be used in point-to-point wireless applications. It is possible to establish a wireless link using antennas with different polarities but network performance and connectivity will suffer.

 

The main advantage or using different antenna polarization schemes is to reduce interference. For example, when mounting several antennas on a tower, it is best to stagger vertically and horizontally polarized antennas to reduce interference.

 

If horizontal or vertical polarization won’t work for your wireless application there are dual-polarized, cross-polarized and circular-polarized antenna options to explore.

 

Dual-polarized antennas feature two antenna elements in a single physical package (radome), one that is vertically polarized and one that is horizontally polarized. When properly installed, dual-polarized antennas can communicate with both vertically and horizontally polarized antennas. An advantage of a dual-polarity antenna is that you essentially get two antennas in one package which saves space and money. These antennas are often used with Multiple-in/Multiple-out (MIMO) wireless access points and CPE devices.

 

Cross-polarized antennas, sometimes referred to as X-Pol antennas, feature two elements in one package. One element is +45° polarized and the other is -45° polarized. The two opposing 45° angle of the elements produce a cross, or “X” orientation. Using a cross-polarized antenna with vertically and horizontally polarized antennas further reduces interference.

 

Circular-polarized antennas have equal response to either horizontal or vertical-polarized antennas. These antennas are designed to either support right hand or left hand polarization to suit varied wireless connectivity applications. Using a circular-polarized antenna on a fixed access point can be beneficial if the linear-polarized remote links are constantly moving.

 

Antenna Polarization Options:

Making sure your antennas are correctly installed and using the proper polarity schemes is crucial to achieving optimal network performance.

 

To learn more about antenna polarization, check out this informative video.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845