Case Study: HBM SoMat

March 8, 2018 at 8:00 AM

 

For more than 65 years, our customer HBM has provided precise and reliable products for a variety of test and measurement applications across a wide range of industries. HBM’s SoMat product line is an innovative portfoloio of precision data acquisition systems for field and lab analysis. Across industries including aerospace, automotive, oil and gas and everything in between, SoMat products  have helped companies by delivering rugged and modular data acquisition systems able to perform a range of on-board data processing while enduring harsh environments.

 

This issue HBM was having was finding a durable, custom interface cable solution at a competitive price for its SoMat product line. Their current cable did not provide the strain relief that was required by its customers. SoMat products used cables that had assembled backshells and because of the non-uniform shape of the cable bundle, the cables were pulling out of the backshell. This flaw was costing the company in product returns and repairs, and leaving customers unhappy.

 

L-com provided HBM with several custom engineered D-subminiature cable assemblies with molded backshells (similar to the one shown here) that were able to replace the existing assemblies. L-com’s cables solved the strain relief problem and reduced overall system cost without compromising design requirements, which fully met HBM’s customers’ requirements.

 

To read the full case study, click here.

 

Case Study: Kinki Sharyo

November 30, 2017 at 8:00 AM

 

In metropolitan areas, thousands of people depend on the rail system every day as a primary mode of transportation. Our customer, Kinki Sharyo, has designed and manufactured more than 10,000 railcars and is the leading supplier of low-floor light rail systems in North America. From manufacturing to maintenance, they design a full-range of customized products to meet the needs for each transit system to get people where they need to go safely and reliably.

 

After being awarded a $30 million contract from NJ Transit, Kinki Sharyo needed to make 60 new trains with DVI, Cat5e and USB cabling for onboard video and LED lighting systems. The problem they were having was finding a cable that could provide connectivity to articulated train cars that are connected to each other.  The existing connectivity method used heavy gauge cables bundled together that frequently wore out and had failure at friction points. They needed a robust cabling system that would not wear down and could withstand the movement of the train cars and constant flexing of the cables.

 

L-com provided Kinki Sharyo with crush-proof armored USB, right-angle Cat5e Ethernet and right-angle DVI cables all off-the-shelf and ready for installation. These cables met all the needs of the new rail car design. The USB cables were more than rugged enough, the right-angle DVI and Cat5e cables were the perfect fit for rail cars with limited space and they all provided the added benefit of low-smoke zero-halogen jackets to protect the new rail cars and passengers inside.

 

To read the full case study, click here.

 

HDMI & DVI - Your Questions Answered

October 5, 2017 at 8:00 AM

 

HDMI and DVI cables are the two most popular video cables used today. Both HDMI and DVI far outperform traditional VGA cables cables that only transmit analog video signals. These digital interconnects are used to link everything from desktop computers and LCD monitors to HDTV’s and entertainment sysyems.

 

DVI is commonly used to connect computers to monitors. They are the most similar to traditional VGA with 24 pins that support analog and digital video. DVI can stream up to 1920x1200 HD video pixels, or up to 2560x1600 pixels using dual-link DVI technology. If the DVI cable or port does not have all 24 pins, it is designed for lower resolution devices, but as long as all the pins are accounted for, it should be able to support the maximum resolution. One downfall of DVI is that it doesn’t support HDCP encryption by default, which means you may not be able to play full HD Blu-rays or other HD content if your harware only includes DVI ports.

 

HDMI is the standard cable used on newer HDTVs, Blu-ray players, Apple TVs, computers and many other video devices. HDMI cables and ports are easy to use and connect with no pins to align, it’s a simple plug and play connection similar to USB. These cables can stream both digital video and audio at the same time. They support up to 1920x1200 HD video and 8 channel audio, as well as HDCP for the newest HD content. HDMI is the first industry supported, uncompressed, all digital audio/video interface and is backwards compatible with DVI-D.

 

 

Still have questions? Here are some of the most frequently asked questions our support team gets asked about HDMI and DVI:

 

 -  What is the maximum length for a DVI cable?

  •    A DVI-D signal can travel 5 meters over a single cable. For distances longer than 5 meters, a DVI extender/repeater is needed.

 

 -  What is the maximum length for an HDMI cable?

  •    A HDMI signal can travel 5 meters over a single 28 AWG cable. A HDMI extender/repeater is needed for distances longer than 5    meters.

 

 -  When using a long HDMI cable, the monitor display is blank or the resolution looks bad. Why?

  •   Currently, HDMI cables up to 5 meters in length will operate properly. If the cable is longer than 5 meters, the signal begins to       degrade and a signal extender is needed.

 

 -  Can I get a HDMI to DVI adaptor?

  •   HDMI is only compatible with single-link DVI-D and single-link DVI-I. It is not compatible with DVI-A, dual-link DVI-D or dual-link      DVI-I, the adaptors will plug-in but will not work for these formats.

 

 -  Can I get a HDMI to VGA adaptor?

  •   No, HDMI is not compatible with VGA.

 

Posted in: Wired

Tags: , , , , , ,

Video Blog- L-com's Toughest Cable Field Test

November 3, 2016 at 8:00 AM

 

Have you ever wanted to test your cables and really push them to the limit? If so, we have a video you MUST watch. We wanted to see just how much abuse our metal armored cables could endure, so we put them through our toughest test ever.

 

Our series of metal armored cables are capable of withstanding the harshest environments and are specifically designed for outdoor, industrial and military applications. Rugged metal armor protects the cable from damage and provides up to 1,500 pounds per square inch (PSI) of crush resistance. The metal jacket also secures the cable from dust, oil, moisture and UV damage. These cables can be used in a variety of industrial applications including factory automation, manufacturing and chemical or petroleum processing networks.

 

Our metal armored cables are currently available off-the-shelf in USB, DVI, HDMI, Ethernet (RJ45) and D-Subminiature styles. Plastic armored cable assemblies with up to 800 PSI of crush resistance are also available. In addition to our extensive off-the-shelf armored cable offering, we can also design and manufacture armored cables to your specifications.

 

Now, check out the video to watch our field test and see just how tough our armored cables are.

 

 

For more videos, tips and tutorials, click here.

 

DisplayPort Connectivity Primer: What You Need To Know

October 20, 2013 at 8:45 AM

 

You may wonder why there’s a need for DisplayPort when HDMI® is as ubiquitous as it is, and with all of its capabilities above traditional analog video.

 

Well, DisplayPort is similar to HDMI® in a lot of ways: smaller connectors, digital video, audio/video on one cable, high definition video, 3D capabilities, etc. For most consumers, especially in the home theater market, if they plug it in and get a display on the screen then it works! And little else matters. As you'll see, however, not all audio/video applications are the same.

 

DisplayPort wasn't necessarily developed to improve on HDMI®, so when we compare HDMI® to DisplayPort, we're not saying it should be either/or. Instead, we're saying before you assume all the personnel in your business need HDMI®-only video cards and laptops, consider taking a look at DisplayPort's capabilities.

 Close Up View of DisplayPort Connector

HDMI® vs. DisplayPort

 

 

HDMI® is in many ways the successor to DVI, which was in many ways the bridge between analog video like VGA and digital video. Improving on DVI, HDMI® includes audio with the video in one cable, does away with the screw locks, and can provide up to 1080p HD video which is necessary for most of the latest TVs used in home theater applications. That's really what HDMI® was developed for and it does a great job.

 

DisplayPort was developed by VESA (Video Electronics Standards Association) as a standard for higher resolution computer display devices. It has most of the features of HDMI® plus some capabilities that are important for the high-graphic demands of some business applications.


Among the top benefits of DisplayPort are:

 

1. Unlike HDMI®, which does not support a very good refresh rate at the higher resolutions, DisplayPort maxes out at 3840 x 2160 pixels with a refresh rate of 60Hz, allowing it to handle very demanding video and 3D applications.


2. The DisplayPort standard can support multiple monitors (up to 4) with a single card, each receiving independent audio/video streams. This is important for individuals working on high resolution graphics, but needing more than one screen to handle the different tool bars or multiple applications running at the same time. In some cases, monitors may be "daisy chained" together, simplifying the setup.


3. DisplayPort has some other minor benefits such as longer cable lengths and a latching feature that makes them more secure in vibration applications than HDMI®'s friction fit connectors.Engineering Drawing of a DisplayPort Connector Calling Out Latches

4. Though DisplayPort is nowhere near as common as HDMI® for peripherals, that is changing. For instance, Thunderbolt, the standard developed by Intel based on the DisplayPort standard, is present on nearly all of Apple's MacBooks and other laptops and computers. Manufacturers of peripherals to be used on MacBooks and elsewhere are designing in either Thunderbolt or Mini DisplayPort to comply.

 

HDMI® isn't going away. Nor should it! It works great for the vast majority of applications. However, there are several applications that will benefit from DisplayPort. In time the technology for DisplayPort will probably be as relevant for those applications as HDMI® is for home theater.

 

 

Posted in: Wired

Tags: , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845