Future-Proofing with Cat6a

August 8, 2019 at 8:00 AM

 

There is no telling what technological breakthroughs await us in the future. But one thing no one wants, is to have to re-cable an entire network because the existing cabling can’t meet the speed and bandwidth needed to support future technology. Re-cabling consumes time, money and a lot of resources. So what is one to do to future-proof their cabling? For many, Cat6a is the answer.

 

Cat6a cables are high-tech cables with advanced performance standards for twisted pair cable systems that offer features surpassing other category cables. They offer more power, faster speeds, tighter twists, further distances, better shielding and greater assurance that they’ll be able to keep up with today’s technology and future advancements. Cat6a cables are able to support upcoming advances in technologies such as Power over Ethernet (PoE), bandwidth-intensive applications and data transfers up to 10 Gbps. With 23-gauge twisted pair, they can transmit those 10 Gbps speeds over distances of up to 100m. Cat6a cables also feature shielding to control interference and crosstalk, which improves performance and increases operational bandwidth. While the extra shielding might add bulk to the cabling, the benefits of Cat6a far outweigh the increased costs that go along with a heavier cable.

 

In addition to PoE, there is a long list of technology coming to market that will continue to increase the need for speed and power. For example, next generation Wave 2 Wi-Fi devices will require 4 Gbps speeds in the near future. Enterprise businesses upgrading to this technology will be able to count on Cat6a to provide the speeds needed. HDBaseT is another emerging technology that would require Cat6a capabilities to transmit full, high definition video, audio and data files over 100 meters. Plus, Cat6a cables can manage the data load needed to support IP convergence, which is beneficial to enterprise networking applications.

 

Overall, Cat6a might cost a bit more than Cat5e or Cat6, but investing in Cat6a now and its ability to keep up with the changing demands of new technology will save money in the long run. Check out our extensive selection of Cat6a cable assemblies.

 

Category 7 Overview

April 4, 2019 at 8:00 AM

 

In today’s world, the need to transfer vast amounts of data at high speeds is required. In many Enterprise datacenters, fiber is sometimes used to handle this task but the price of expensive optics and other factors might require a copper based solution.

 

Enter Category 7 cables!

 

Category 7’s most notable quality is its capability of handle speeds of up to 10 Gbps over 100 meters, especially when compared to Cat6 and Cat5e’s 1 Gbps speeds over the same distance. During testing, speeds of up to 40 Gbps have been measured over a distance of 50 meters, and up to 100 Gbps over 15 meters. And, Cat7 cables are able to deliver those high speeds at a higher frequency of 600 MHz, as opposed to Cat6a’s max frequency of 500 MHz. This means that a Cat7 cable will be able to transfer data faster than any of the previous category cables, making it an ideal option for wiring smart homes, data centers, large enterprise networks or anywhere else a high-speed wired connection is required.

 

Aside from speed, Cat7’s other benefits of note include the extensive shielding of its twisted pairs which can considerably reduce signal attenuation and improve noise resistance. The individual pairs in these cables are shielded with an additional layer of shielding over the whole cable.

 

Cat7 cables are also extremely durable and generally have a longer lifespan that Cat5 and Cat6 cables. And while Cat7 cables can be more expensive than other category cables, that price can be offset by their increased performance and resilience.

 

Cat7 has a good amount of admirable qualities and with it being backward compatible with traditional Cat5 and Cat6 cables, Category 7 might be the right choice for your next wired installation. If your application is outdoors or in an industrial environment, check out our new rugged, Cat7 cables with 10 Gig rating. 

 

Readers’ Choice -Top Blog Posts of 2018

December 20, 2018 at 8:00 AM

 

Our goal for this blog is to provide interesting and informative content for our readers. So we always enjoy taking a look back at the end of the year to see what the most popular posts were. To make sure you didn’t miss anything, here’s a list of the most read posts of 2018. We hope to see you back in 2019!

 

 

1.      Cat6 Cable: Shielded vs. Unshielded


Category 6 Ethernet cable is designed to provide high speed data rates, but how do you decide between shielded or unshielded? Here, we compare them side by side so you can choose which will work best for your application. Read more.

 

 

2.      10 of the Worst Cabling Nightmares

 

We pride ourselves on our commitment to provide the best connectivity solutions for our customers, helping them to manage their data centers. So it always comes as a shock when we see cabling infrastructure that is a complete nightmare. This post has some of the worst offenders we’ve seen on the web. Read more.

 

 

3.      The Advantages and Disadvantages of Shielded Ethernet Cable

 

When it comes to shielded Ethernet cable, there are pros and cons. This post takes a look at both the good and the bad to help you weigh your options. For example, shielding can offer protection from EMI/RFI but its weight and limited flexibility means it’s not ideal for every application. To help decide if shielded Ethernet cable is right for your installation, read the post.

 

 

4.      75 Ohm vs. 50 Ohm – Coaxial Comparison

 

Ohm may sound like something you’d say while meditating, but when it comes to coaxial cables, it is actually a unit of resistance. Ohms measure the impedance within the cable. Impedance is resistance to the flow of electrical current through a circuit. To see how 75 Ohm and 50 Ohm compare, read our post.

 

 

5.      Good Vibrations: Vibration-Proof USB Connectors


Universal Serial Bus (USB) is one of the most widely used technologies to connect and power devices. One fundamental flaw of USB is its sensitivity to vibration, causing the connector to dislodge. In this post we show you some solutions to keeping your USB connected. Read more.

 

Readers’ Choice -Top Blog Posts of 2017

December 21, 2017 at 8:00 AM

 

As we wrap up another year, we’d like to take a moment to look back on some of our most popular posts. We pride ourselves on providing informative content for our readers by covering a range of wired and wireless technology topics. We sincerely hope that you enjoyed reading our posts as much as we enjoyed writing them and in case you missed anything, here’s a highlight reel of the most popular posts of 2017.

 

 1.       Cable Showdown: Cat6 vs. Cat6a

 

It’s a Cat eat Cat world out there and Cat6 and Cat6a are two of the most popular standards for Ethernet cables. So, how do you decide between the two? One may work better than the other, depending on your application. To help you pick a winner, we compared them side-by-side for a showdown of category proportions. To see how each Cat fared, read the post.

 

 

2.       White-Space Wi-Fi 802.11af

 

Waste not, want not, seems to be a growing way of life for many people these days, and that theme will soon apply to the Wi-Fi spectrum as well. The IEEE standard 802.11af, also known as white-space Wi-Fi or White-Fi, will utilize the unused space in the TV spectrum, the TV white-space, to support Wi-Fi networks. Read the post to find out how it all works.

 

 

3.       OM5 – The Next Generation of Multimode Fiber

 

OM5 was chosen to be the new standard for cabling containing wideband multimode fiber in the 3rd edition of the ISO/IEC 11801 standard. The acceptance of this standard is a milestone for the fiber cabling performance category because it extends the benefits of this revolutionary multimode fiber within connected buildings and data centers worldwide. To find what you need to know about OM5, click here.

 

 

4.       802.11ax – The Next Big Thing

 

The IEEE will be adding to its 802.11 series of standards again with the launch of 802.11ax. 802.11ax is under development and will pick-up where 802.11ac left off by taking MIMO to the next level with MIMO-OFDM. This next big upgrade to Wi-Fi networks might not make its debut for a couple of years, but here’s a look at what’s coming.

 

 

5.       75 Ohm vs. 50 Ohm – Coaxial Comparison

 

Ohm may sound like something you’d say while meditating, but when it comes to coaxial cables, it is actually a unit of resistance. Ohms measure the impedance within the cable. Impedance is resistance to the flow of electrical current through a circuit. To see how 75 Ohm and 50 Ohm compare, read our post.

 

 

How to Protect Your Equipment During Lightning Season

August 24, 2017 at 8:00 AM

 

No matter how lucky you are, the thought of lightning striking your expensive communications equipment can be a scary thought. Depending on your location, the time of year and your proximity to other buildings, the chances of a lightning strike can be higher or lower, but any lightning strike can be debilitating for sensitive electronic equipment. Both direct and indirect strikes can cause extensive damage that includes loss of data, downtime and the cost of replacement.

 

Electromagnetic fields and earth-voltage spikes caused by lightning can also wreak havoc on electronic power and signal circuits. This can damage the Ethernet, coaxial and telephone lines, or anything connected to the circuits. Even entire campuses can experience long-range voltage spikes that can ruin all electronics connected by the above-ground and below-ground cabling systems that run throughout the campus.

 

There’s no single cure-all method, but lightning protectors are an inexpensive way to help protect equipment in the event of a lightning strike. Here are some of the best solutions to give your equipment a fighting chance:

 

 

Coaxial Protectors – These lightning protectors use gas-filled tubes to discharge electrical spikes before they can cause damage. They are used in both wired and wireless networks to protect radios, communications equipment and anything else attached to coaxial cable, which becomes a target for lightning. They feature popular connector types including N, TNC, RP-BNC and F.

 

Low-PIM Coaxial Protectors – Theses are ideal for use with Distributed Antenna Systems (DAS) because of their low-PIM performance of -150dBc. They feature bi-directional protection and there are no gas tubes to replace.

 

Cat5/5e/6 and PoE Protectors – These protectors ground-out and discharge spikes that can permanently blackout security cameras, switches routers and other critical equipment. They are ideal for 10/100/1000 Base-T Ethernet networks. Some models even feature integral PoE injectors that can deliver remote power to access points, access servers, outdoor routers and other Ethernet IP enabled devices.

 

Telephone/DSL/T1 Protectors – They protectors can prevent your POTS or other telephone system from expensive downtime and are perfect for indoor or outdoor installations. These protectors are available in multiple styles including screw terminal 

and RJ11 options.

 

RS232/422/485 Protectors – These are ideal for protecting RS-232, RS-422 and RS-485 lines. They can also save sensors, control lines and AISG lines from lightning’s damaging effects.

 

To see all the products L-com offers to protect your equipment from lightning, click here.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845