What You Need to Know About 802.11ay

November 9, 2017 at 8:00 AM

 

Products for 802.11ad have only begun hitting the market in the past year, and already the IEEE is working on improvements in the form of 802.11ay. This new and improved standard will expand upon 802.11ad technology by delivering faster and longer-range Wi-Fi networks. Expected to be released in late 2019, 802.11ay will increase bandwidth and improve the reliability and robustness of the unlicensed 60GHz millimeter wave spectrum. It will be designed to improve throughput, range and use-cases.

 

The next generation wireless standard promises significant improvements upon the 7 Gbps speed and 10-meter distance capabilities of 802.11ad. 802.11ay will be capable of transmission rates of 20 to 30 Gbps and distances of 30 meters with 11ay-to-11ay device setups. When channel bonding, MIMO and additional capabilities are added into the mix, it’s possible that 802.11ay will deliver speeds closer to 200 Gbps and extend transmission distances up to 300 meters.

  

As an amendment for improving the performance of the 802.11ad standard, 802.11ay will support the same broad applications and be backward compatible with the 802.11ad standard. 802.11ay will focus on new applications for mobile offloading, wireless docking and display connectivity. It will also be ideal for fixed point-to-point or point-to-multipoint outdoor backhaul applications. 802.11ay might also be used in internal mesh and backbone networks, to provide connectivity to VR headsets, support server backups and manage cloud applications that require low latency. The main targets for 802.11ay are DisplayPort, HDMI and USB connectivity, fast synch as well as short-range, high-bandwidth connectivity to TV and monitor displays. It could even act as a replacement for HDMI and USB and make the equipment more intuitive.

 

802.11ay is primed to pack a punch with super-charged 20 Gig speeds and greater transmission distance. This revolutionary IEEE standard will surely break records and set the standard for future wireless technology.

 

Standards Showdown: 802.11 Standards Side-by-Side

July 20, 2017 at 8:00 AM

 

The IEEE is almost always working on another new amendment to the 802.11 Wi-Fi standard. We now have nearly as many 802.11 standards as there are letters in the alphabet, and keeping them straight can get confusing. Fortunately, we’ve compiled a comprehensive list of all of the 802.11 standards, old and new, for easy reference. 

 

Readers' Choice -Top Blog Posts of 2016

December 29, 2016 at 8:00 AM

 

As another year comes to a close, so does another chapter of our blog, Engineering Hub. We covered a wide variety of topics in order to keep you, our readers, in the loop with what’s going on in the world of wired and wireless technology. Here are highlights of the 2016 posts that were the most popular with our readers.

 


1.       802.11ay: 20 Gig Wireless!


The next generation wireless standard will blow you away with triple the speed and 30xs the transmission distance of 802.11ad. Learn about all of the benefits of 802.11ay and what it means for the world of wireless networking technology. (Read more)

 

 

 

2.       Fiber Showdown: Multimode vs. Single mode


Multimode and single mode are the two most common types of fiber optic cables. Both have very different attributes and one may work better than the other, depending on the needs of your application. This post will help you decide which will give you the best results. (Read more)

 

 

 

3.       Cat6 Cable: Shielded vs. Unshielded


Category 6 Ethernet cable is designed to provide high speed data rates, but how do you decide between shielded or unshielded? Here, we compare them side by side so you can choose which will work best for your application. (Read more)

 

 

 

4.       Good Vibrations: Vibration-Proof USB Connectors

 

Universal Serial Bus (USB) is one of the most widely used technologies to connect and power devices. One fundamental flaw of USB is its sensitivity to vibration, causing the connector to dislodge. In this post we show you some solutions to keeping your USB connected. (Read more)

 

 

 

5.      Next Generation Positioning: A look at what’s around the corner

 

GPS apps and positioning technology is something we use everyday to get directions or find something or someone nearby, and that usage is expected to continue to grow at a staggering rate. Here’s a look at what the IEEE has in store for next gen positioning technology. (Read more)

802.11ay: 20Gig Wireless!

March 31, 2016 at 8:00 AM

 

Hold on to your hats – or in this case, your wireless devices – and prepare to be blown away by 802.11ay. The next generation wireless standard promises almost three times the speed of 802.11ad with transmission rates of 20 Gbps, up from 802.11ad’s current rate of  7 Gbps. It will also extend transmission distance from the 10 meter limit of 802.11ad to as far as 300-500 meters!

 

Scheduled for release next year, 802.11ay will increase bandwidth and improve the reliability and robustness of the 60GHz millimeter wave spectrum. It will be designed to improve throughput, range and use-cases.

 

The focus of 802.11ay will be on new applications for mobile offloading, wireless docking and display as well as indoor and outdoor wireless backhaul. It is also expected to include mechanisms for MU-MIMO and channel bonding technologies.

 

The main targets for 802.11ay are DisplayPort, HDMI and USB connectivity, fast synch as well as short-range, high-bandwidth connectivity to TV and monitor displays.  

 

As an amendment for improving the performance of the 802.11ad standard, 802.11ay will support the same broad applications and be backward compatible with the 802.11ad standard.

 

802.11ay is primed to pack a punch with super-charged 20 Gig speeds and greater transmission distance. This revolutionary IEEE standard will surely break records and set the standard for future wireless technology.

 

Posted in: Wireless

Tags: , , ,

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845