802.11ad - What is WiGig?

November 15, 2018 at 8:00 AM

 

As the evolution of wireless technology continues, so does the development of new wireless standards. Next on the list is 802.11ad – also known as WiGig. Most of the emerging wireless standards have been a steady progression, but this one has some fundamental changes planned. Here, we’ll explore what WiGig is all about.

 

As far as speed is considered, WiGig will support data rates up to 7 Gbps, though real data rates might be less than this maximum limit. WiGig operates on the 60 GHz frequency, as opposed to Wi-Fi which uses the 2.4 to 5 GHz bands. This should result in much less congestion compared to Wi-Fi’s congested frequencies and WiGig also shouldn’t have as many interference issues as there are on the 2.4 GHz Wi-Fi band. Plus, it utilizes a narrow signal beam to reduce attenuation. But with a range of only around 30 feet and the 60 GHz signal unable to penetrate obstacles, WiGig is limited to one room with a clear line of sight from the transmitter to the receiver.

 

Instead of MIMO, WiGig uses multiple antennas for beamforming, which helps reduce attenuation. WiGig beamforming utilizes a phased antenna array that provides a signal power boost in whichever direction it is aimed. One of these access points can have as many as 64 antennas to generate up to 128 beams.

 

For multiple access, Service Period (SP), a new channel access mode, has been added to WiGig. This creates transmission schedules that are assigned to clients by access points. Time on the channel is organized into intervals called Beacon Intervals (BI). SP access is projected to be the preferred channel access in WiGig.

 

WiGig will also introduce a new mode of operation called PBSS. With PBSS, there is a central coordinator, like an access point (AP), but it allows clients to communicate while surpassing the AP. Clients can also talk to one another directly with this. PBSS is designed for applications that stream HD video to a display, because it doesn’t require the video to be sent through the AP, but it can still connect through the AP in other areas of the network.

 

In addition to 2.4 and 5 GHz, future Wi-Fi devices are expected to include 60 GHz radios and are expected to be capable of seamless transfers between the bands. Not only is WiGig bringing something new to today’s wireless networks, but it will add extra capability to future applications.

 

How the IoT is Affecting Wi-Fi

October 18, 2018 at 8:00 AM

 

In today’s society, Wi-Fi has become something that people now expect to be readily available and depend on to carry out everyday tasks. With the rollout of the Internet of Things (IoT), people will soon become accustomed to having all of their things connected as well. But with all of those connected devices, can Wi-Fi handle an even greater influx of user demand for high-speed connectivity? Here, we’ll take a look at how the IoT is affecting Wi-Fi.

 

When it comes to connectivity requirements, each IoT application can have a different set of range, data throughput and energy efficiency needs. Some IoT devices only need small, intermittent data transfers, such as utility meters. While some need a constant stream of data, such as live surveillance cameras. Also, range can differentiate from very short for wearables, to spanning miles for weather and agricultural sensor applications. But there are two things that are constants for all IoT applications: the need for remote power and constant connectivity.

 

To fulfill this need, Wi-Fi is the obvious choice because Wi-Fi coverage is so widespread, but standard Wi-Fi is not always the best choice for IoT applications. Thus, there are several standards that have emerged from the need for IoT connectivity. These include LoRaWAN, multiple short range communications standards and new Wi-Fi standards such as HaLow (802.11ah) and HEW (802.11ax).

 

The 802.11ah standard was introduced to address the range and power needs of the IoT. It utilizes the 900 MHz frequency band to provide extended range, covering a one kilometer radius, lower power requirements, wake/sleep periods and station grouping options.

 

The 802.11ax standard also includes the wake/sleep and station grouping features, and has a MU-MIMO feature that allows up to 18 users to simultaneously send data within a 40 MHz channel when paired with the smaller subcarrier spacing. Internet service providers and technology startups have also begun developing an application layer that includes mesh networks that use sets of routers to work together and extend wireless coverage, and provisioning tactics that define how wireless devices connect to networks.

 

There is some fear that the IoT could essentially break Wi-Fi, but there seems to be plenty of development activity focused around finding solutions to Wi-Fi congestion before it becomes a problem. With all of the IoT devices expected to be connecting in the near future, there will likely be a significant shift in Wi-Fi practices and standards, but as with everything in the world of technology, being able to pivot and reconfigure is the name of the game.

 

Readers’ Choice -Top Blog Posts of 2017

December 21, 2017 at 8:00 AM

 

As we wrap up another year, we’d like to take a moment to look back on some of our most popular posts. We pride ourselves on providing informative content for our readers by covering a range of wired and wireless technology topics. We sincerely hope that you enjoyed reading our posts as much as we enjoyed writing them and in case you missed anything, here’s a highlight reel of the most popular posts of 2017.

 

 1.       Cable Showdown: Cat6 vs. Cat6a

 

It’s a Cat eat Cat world out there and Cat6 and Cat6a are two of the most popular standards for Ethernet cables. So, how do you decide between the two? One may work better than the other, depending on your application. To help you pick a winner, we compared them side-by-side for a showdown of category proportions. To see how each Cat fared, read the post.

 

 

2.       White-Space Wi-Fi 802.11af

 

Waste not, want not, seems to be a growing way of life for many people these days, and that theme will soon apply to the Wi-Fi spectrum as well. The IEEE standard 802.11af, also known as white-space Wi-Fi or White-Fi, will utilize the unused space in the TV spectrum, the TV white-space, to support Wi-Fi networks. Read the post to find out how it all works.

 

 

3.       OM5 – The Next Generation of Multimode Fiber

 

OM5 was chosen to be the new standard for cabling containing wideband multimode fiber in the 3rd edition of the ISO/IEC 11801 standard. The acceptance of this standard is a milestone for the fiber cabling performance category because it extends the benefits of this revolutionary multimode fiber within connected buildings and data centers worldwide. To find what you need to know about OM5, click here.

 

 

4.       802.11ax – The Next Big Thing

 

The IEEE will be adding to its 802.11 series of standards again with the launch of 802.11ax. 802.11ax is under development and will pick-up where 802.11ac left off by taking MIMO to the next level with MIMO-OFDM. This next big upgrade to Wi-Fi networks might not make its debut for a couple of years, but here’s a look at what’s coming.

 

 

5.       75 Ohm vs. 50 Ohm – Coaxial Comparison

 

Ohm may sound like something you’d say while meditating, but when it comes to coaxial cables, it is actually a unit of resistance. Ohms measure the impedance within the cable. Impedance is resistance to the flow of electrical current through a circuit. To see how 75 Ohm and 50 Ohm compare, read our post.

 

 

Standards Showdown: 802.11 Standards Side-by-Side

July 20, 2017 at 8:00 AM

 

The IEEE is almost always working on another new amendment to the 802.11 Wi-Fi standard. We now have nearly as many 802.11 standards as there are letters in the alphabet, and keeping them straight can get confusing. Fortunately, we’ve compiled a comprehensive list of all of the 802.11 standards, old and new, for easy reference. 

 

802.11ax - The Next Big Thing

March 2, 2017 at 8:00 AM

 

The IEEE is at it again. Its long-running 802.11 series of standards will be reincarnated yet again with the launch of 802.11ax.  This next big upgrade to Wi-Fi networks might not make its debut for a couple of years, but here’s a look at what is coming.

 

802.11ax is under development and will pick-up where 802.11ac left off by taking MIMO to the next level with MIMO-OFDM. MIMO-OFDM (orthogonal frequency division multiplexing) technology will be capable of subdividing signals even further which ultimately creates a bigger "pipe" to deliver larger volumes of data. This will significantly expand and increase throughput to deliver five times more capability than the gigabit speeds promised by 802.11ac. Lab-based trials of 802.11ax have even hit max speeds of 10.53Gbps, or around 1.4 gigabytes of data transfer per second.

 

As impressive as those speeds sound, 802.11ax is not just focused on being fast; its real focus is high-density Wi-Fi deployments. This means that the goal is not only to improve speed, but to enhance the ability of connections to remain active even when there is heavy interference. This will make the system more efficient with the sophistication to successfully route pieces of messages to their destination. 802.11ax will operate in the 5GHz band, where there is plenty of space for 80MHz and 160MHz channels.

 

Before you get too excited, implementing a new standard is a time-consuming and rigorous process, so we won’t likely see 802.11ax ratified until closer to 2019. Then it will take even more time before certified hardware hits the market.

 

© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, North Andover, MA 01845