Using Latching USB Cables for Vibration-Proof Connections

April 24, 2013 at 10:00 AM


Latching USB Cables

One of the most successful connectivity technologies is Universal Serial Bus or USB 2.0. Why? You can find it everywhere, from laptops and desktop computers to peripheral devices like printers, mice and keyboards, to consumer electronics like cell phones and camcorders. 

 

(Click here for a tutorial on USB technology.)

 

Surprisingly though, there are some fundamental problems with USB 2.0, one of which is its sensitivity to vibration.

Latching USB Drawing

 

USB 2.0 uses what's called a "friction fit" to remain connected, which means the friction between the connector and the jack is all that holds the connection together. As you'd find with vehicles and in military/aerospace applications, vibration can cause connectors to unexpectedly separate.

 

L-com has countered this problem by offering "latching" USB 2.0 cables.  The latches, which are on the sides of the connector, fit into any standard USB 2.0 female jacks.  Currently latches are only available on USB 2.0 Type A male connectors and they come standard on micro-B male connectors. L-com offers:

 

 
 
Quick note: Latching connectors are also available for SATA cables.
 
Additionally, L-com now offers USB 3.0 cables with locking thumbscrews. These cables can be used in machine vision applications or with any application where vibration is an issue.
 

Identifying Array Antennas

April 17, 2013 at 10:00 AM

What are they?


An antenna array is a group of two or more directional (usually panel style) antennas that are grouped together to form an Omni directional signal. Many times an RF splitter is used to connect the multiple antennas to a single access point or WiFi amplifier.

 

The benefit of using an antenna array over a single Omni directional antenna is that the antenna array provides radiation patterns that a single Omni antenna would not. Many times antenna arrays provide greater coverage than a single Omni antenna could.

 

 

Antenna array mounted on a pole RF splitter connected to an antenna array
Antenna array mounted on a pole RF splitter connected to an antenna array

Down tilt mounting feature
Down tilt mounting feature 

 



Where Would You Use Them?


Antenna arrays are used in outdoor point-to-multipoint applications. L-com's antenna arrays are available in 90° (4 panels), 120° ( 3 panels), and 180° (2 panels) configurations and include appropriate splitter and cables. Additionally, these antenna arrays feature zero to 20° down tilt capability to compensate for the geography of the installation location. This helps ensure maximum wireless signal coverage in the service area.

 

 

Antenna Array Configurations Available

 

 

Antenna Arrays with four 90° sectorial antennas Antenna Arrays with four 90° sectorial antennas
Antenna Arrays with three 120° sectorial antennas Antenna Arrays with three 120° sectorial antennas
Antenna Arrays with two 180° sectorial antennas Antenna Arrays with two 180° sectorial antennas
 

All sectorized omni array configurations are designed to all-weather operation. They feature both heavy-duty polymer antenna radomes and stainless steel mounting systems. 

 
  
© L-com, Inc. All Rights Reserved. L-com, Inc., 50 High Street, West Mill, Third Floor, Suite 30, MA 01845